Schmalz

A Firm Grip, Even on Porous Objects

Need to handle airtight, porous or non-rigid components safely using lightweight or small industrial robots? Schmalz has the perfect solution with its new pneumatic vacuum generator RECB.

The new pneumatic vacuum generator RECB is ideal for end-of-arm use on lightweight or small industrial robots.

This robot arm is a vital component in lightweight and industrial robots. Even more important, however, is the interface between the robot arm and the workpiece (for instance, grippers, sensors, or tool changers), because these components are responsible for handling workpieces and products safely. That can be a challenge, for instance, if the objects are porous (like cardboard packaging) or have uneven surfaces. Handling non-rigid objects such as filled cardboard boxes in palletizing and de-palletizing processes can also be difficult.

J. Schmalz GmbH has developed the vacuum generator RECB for exactly such requirements. The RECB can handle workpieces weighing up to ten kilograms. Unlike its sisters from the ECBPi and ECBPMi series, it generates the vacuum purely pneumatically. The new RECB is both particularly compact and extremely powerful, with a suction rate of 59 standard liters per minute. It lets the user implement short cycle and evacuation times in fully automated processes, while also providing the benefit of high leakage compensation. Establishing the mechanical and electrical connection between the vacuum generator and a robot is very simple. Furthermore, its low overall height means it can be mounted directly on the robot arm when height is restricted. The new RCEB is controlled by digital robot outputs, with communication via IO-Link.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku