Schmalz

Specialist for Highly Textured Surfaces

It is not easy to handle workpieces with highly textured surfaces reliably. With the compact flow gripper SCG-HSS, Schmalz has developed an efficient solution for doing so. The solution grips even sensitive workpieces very gently with minimal surface pressure – and low operating costs.

Flow gripper SCG-HSS handling populated printed circuit boards.

Populated printed-circuit boards are a classic example of components that are very difficult to handle due to their heavily textured surface. J. Schmalz GmbH has developed the flow gripper SCG-HSS for just such a task. Since the gripper applies only minimal pressure to the surface of the workpiece, it can gently grip sensitive components, even if they have openings and low population levels. The SCG-HSS handles objects with positional and spatial precision. The Schmalz solution is suitable for small parts – multiple grippers can be combined for larger workpieces.

A pin curtain lets the new flow gripper adapt to the surface contour automatically, allowing it to grip different kinds of workpiece without any additional set-up times. The basic model is made from non-anodized aluminum, which makes the SCG-HSS particularly lightweight. It also features a compact design. The integrated vacuum generation unit is powered by compressed air and achieves a high suction capacity with minimal air consumption, which means the operator benefits from low operating costs. Furthermore, the SCG-HSS has an ESD-compliant design and therefore protects sensitive parts from uncontrolled electrostatic discharge.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku