Schmalz

Výsledky vyhledávání

Výsledky filtrování

Kategorie

1 - 10 z 11 výsledků

Video

Schmalz layer gripper SPZ in the palletizing application

Standard layer gripper SPZ Modular with SPB2 40 silicone suction pad for palletizing entire cardboard layers.Standard layer gripper SPZ Modular with SPB2 40 silicone suction pad for palletizing entire cardboard layers. Includes layer pad and pallet handling module, spring-loaded flange to compensate for layer unevenness and layer detection.

Video

Layer gripping system SPZ for automated handling of cans in layers

In order to implement a logistical process for transporting layers of cans within a packaging process, the company decided to purchase a vacuum layer gripping system from Schmalz. The layer gripping system SPZ can transport complete layers of 90 cans. The system is not bound to a particular can size, meaning that even entire layers of cans with different weights ranging from 16 kg to 34 kg do not represent a problem for the layer gripping system. The patented sealing foam prevents leakage and facilitates heavy holding forces, even for cans on a running conveyor belt.In order to implement a logistical process for transporting layers of cans within a packaging process, the company decided to purchase a vacuum layer gripping system from Schmalz. The layer gripping system SPZ can transport complete layers of 90 cans. The system is not bound to a particular can size, meaning that even entire layers of cans with different weights ranging from 16 kg to 34 kg do not represent a problem for the layer gripping system. The patented sealing foam prevents leakage and facilitates heavy holding forces, even for cans on a running conveyor belt.

Video

Vacuum layer gripping system SPZ for palletizing and depalletizing various product layers

Schmalz has developed a special gripping system to automate the handling of various product layers. The vacuum layer gripping system SPZ consists of modularly connected large-area grippers, which allow for easy adjustment of the gripper to meet individual requirements. The suction area consists of flexible sealing foam which adapts to fit the contours of each workpiece perfectly. The layer gripping system is equipped with check valves, which detect and seal off unused parts of the suction area. This technology enables you to lift small layers or layers with gaps. The integrated vacuum generation provides additional advantages. The gripper can be connected directly to the compressed air supply. No tubing is required to connect it to an external vacuum generator. This simplifies assembly, minimizes part interference and considerably reduces the volume that has to be evacuated. Because the necessary vacuum can be generated faster, this solution also allows for shorter cycle times. The gripper is ideal for dynamic handling processes, and is flexible enough for various applications in areas such as warehousing and intralogistics.Schmalz has developed a special gripping system to automate the handling of various product layers. The vacuum layer gripping system SPZ consists of modularly connected large-area grippers, which allow for easy adjustment of the gripper to meet individual requirements. The suction area consists of flexible sealing foam which adapts to fit the contours of each workpiece perfectly. The layer gripping system is equipped with check valves, which detect and seal off unused parts of the suction area. This technology enables you to lift small layers or layers with gaps. The integrated vacuum generation provides additional advantages. The gripper can be connected directly to the compressed air supply. No tubing is required to connect it to an external vacuum generator. This simplifies assembly, minimizes part interference and considerably reduces the volume that has to be evacuated. Because the necessary vacuum can be generated faster, this solution also allows for shorter cycle times. The gripper is ideal for dynamic handling processes, and is flexible enough for various applications in areas such as warehousing and intralogistics.

Video

Layer gripping system SPZ with combi foam for layerwise handling of cans

Layers of cans are palletized and depalletized as part of a logistics process. Handling layers of cans is a particularly challenging task due to the round edge of the workpiece. As a solution for this problem, Schmalz offers the layer gripping system SPZ with combination foam. The vacuum layer gripping system SPZ consists of modular, locked large-area vacuum grippers and allows the handling of complete product layers. In this application the vacuum layer gripping system SPZ is equipped with a special combi foam which is one out of three possible sealing plates. The patented combi foam with its innovative layer structure is especially used for the handling of workpieces with small diameters, such as cans with a continuous edge or glass and buckets.Layers of cans are palletized and depalletized as part of a logistics process. Handling layers of cans is a particularly challenging task due to the round edge of the workpiece. As a solution for this problem, Schmalz offers the layer gripping system SPZ with combination foam. The vacuum layer gripping system SPZ consists of modular, locked large-area vacuum grippers and allows the handling of complete product layers. In this application the vacuum layer gripping system SPZ is equipped with a special combi foam which is one out of three possible sealing plates. The patented combi foam with its innovative layer structure is especially used for the handling of workpieces with small diameters, such as cans with a continuous edge or glass and buckets.

Video

Vacuum Layer Gripping System SPZ for flexible Handling of different Layers of Cans

During the manufacture of cans, entire layers of opened cans need to be taken from a roller belt and stacked on a pallet. With a layer gripping system from Schmalz, this process can be performed quickly and efficiently. The vacuum layer gripping system SPZ is suitable for product layers with a variety of sizes and structures. This makes the layer gripper ideal for use in warehouse logistics and intra-logistics. The dimensions of the layer gripping system were designed especially to meet customer requirements. In order to handle empty cans, the gripper system has to evacuate the empty space. This enables the workpieces to be handled quickly and efficiently. The gripper system is equipped with special flexible foam for optimum adaptation to the workpiece structure, ensuring gentle handling of the products. This means no gripper change is necessary for heterogeneous workpieces, which eliminates the time and money that would otherwise be spent when a new order came in. The custom gripper system was also designed to allow use even when the gripper is only partially covered.During the manufacture of cans, entire layers of opened cans need to be taken from a roller belt and stacked on a pallet. With a layer gripping system from Schmalz, this process can be performed quickly and efficiently. The vacuum layer gripping system SPZ is suitable for product layers with a variety of sizes and structures. This makes the layer gripper ideal for use in warehouse logistics and intra-logistics. The dimensions of the layer gripping system were designed especially to meet customer requirements. In order to handle empty cans, the gripper system has to evacuate the empty space. This enables the workpieces to be handled quickly and efficiently. The gripper system is equipped with special flexible foam for optimum adaptation to the workpiece structure, ensuring gentle handling of the products. This means no gripper change is necessary for heterogeneous workpieces, which eliminates the time and money that would otherwise be spent when a new order came in. The custom gripper system was also designed to allow use even when the gripper is only partially covered.

Slovníček

Gripping Systems

Gripping systems from Schmalz can be used in all areas of automated handling. The gripping systems are customized to customer's needs.Gripping systems from Schmalz are used in automated handling processes in different industries, such as packaging, wood or intralogistics.Gripping Systems are used in all areas of automatic handling. Application areas of Schmalz gripping systems are for example handling of wood, packaging and cardboard as well as intralogistics and sheet metal forming. Gripping systems from Schmalz operate with vacuum. Therefore, they are called vacuum gripping systems. They are divided in four different product categories: Area gripping systems, vacuum layer gripping systems, vacuum suction spiders and vacuum end effectors. Gripping systems from Schmalz are adapted individually to the application of the customer and projected in cooperation with our Schmalz product experts.Area Gripping Systems for Automated ProcessesThe area gripping systems FXP and FMP from Schmalz persuade with great flexibility. The gripping systems allow applications such as automatic palletizing, depalletizing, commissioning and sorting of different workpieces. Due to their unique suction force area gripping systems are suitable for a lot of different workpiece sizes and materials. Cardboard, wood, metal sheets, plastics and even workpieces with openings can be handled effortlessly. The advantages are obvious: Little tare weight allows maximum process acceleration and lowers the system costs at the same time because smaller robots can be used. The flow-optimized design lowers operation costs long-lasting and with the integrated silencer the sound level is reduced to 74 dB (A). When handling compact workpieces, the gripping systems FX and FM can be used as well. They enlarge the handling spectrum of the bigger FXP/FMP downwards and demonstrate impressively the flexibility of the gripping system portfolio. Area gripping systems from Schmalz are equipped with either an integrated vacuum generator or connection valves for an external vacuum source depending on the customers’ request.Vacuum Layer Gripping Systems for Warehouse Logistics and IntralogisticsVacuum layer gripping systems SPZ from Schmalz increase the productive capacity during the automatic handling of products and workpieces in many industries. Application areas of layer gripping systems from Schmalz are for example palletizing and depalletizing in layers of a wide range of goods or the use in warehouse and intralogistics. The layer gripping system SPZ allows the handling of layers with gaps, mixed layers, intermediate layers, pallets, cardboard packaging and film packaging. Due to an innovative combination of vacuum technology and mechanical support even incomplete pallets can be loaded and unloaded. For typical applications in certain industries Schmalz developed industry-specific layer gripping systems: The gripping system SPZ Glass handles layers of glasses and cans, while the gripping system SPZ Packaging palletizes and depalletizes cardboards or beverage trays. The SPZ Logistics is used in warehouse logistics and intralogistics and handles various product layers. For the de-stacking of cut-optimized wooden or metal sheets the gripping system SPZ Nesting was developed. Schmalz offers for its layer gripping systems a wide range of accessories. An optional sensor unit optimizes cycle times. Vacuum-detection and part monitoring increase the process security. To protect from collisions it is possible to build in a collision monitoring in the floating attachment of the gripping system. The optional frequency converter enables to regulate the blower independent from workpiece and process. As a result the energy consumption of the gripping system can be reduced by thirty to seventy percent. The special deep-freezing design is recommended, for applications where the temperature is very low (up to -30°C).Customized Gripping SystemsThe vacuum suction spider SSP forms the basis for the customized solutions for end-of-arm-tooling from Schmalz. Thanks to the extensive catalogue with over 3.500 standardized vacuum components the gripping system can be configured for the particular application. Thereby, the application areas of the gripping system SSP are versatile: It is used in automation of handling flows in manufacturing, assembly and quality control processes, in linking robots in presses and bending centers and automation of plastic injection molding machines, deep drawing machines, laser machines and punching maschines. The materials a gripping system SSP can handle are versatile: Metal sections, blanks, stone, sheet materials, car body parts, glass and ceramic components, solar panels and so on.Gripping Systems for Highspeed Packaging ProcessesFor pick and place applications with delta, scara or articulated-arm robots Schmalz developed the vacuum end effector VEE. The gripping system is used for fully automatic filling of cardboard boxes in case packers or in primary and secondary packaging processes. Thanks to a unique flexibility the gripping system VEE is suitable for the usage in flexible packaging machines with frequent changes of the format. The vacuum end effector VEE can be equipped with a great number of different suction cups which allows the handling of various materials.

Tisková zpráva

New lightweight layer gripper ZLW: slim for the cobot

With the new weight-reduced layer gripper from Schmalz, cobots can also palletize lighter workpiece layers. It is not only slim, but also efficient: Schmalz optimally matches the suction grid, gripper dimensions and all other components to the handling task, thus minimizing the power required for vacuum generation.With the new weight-reduced layer gripper from Schmalz, cobots can also palletize lighter workpiece layers. It is not only slim, but also efficient: Schmalz optimally matches the suction grid, gripper dimensions and all other components to the handling task, thus minimizing the power required for vacuum generation.Depending on the model and manufacturer, lightweight robots have a payload of up to 25 kilograms. In order to use them for layer-by-layer palletizing and depalletizing, J. Schmalz GmbH has given its layer grippers a diet. The result is the particularly lightweight layer gripper ZLW, which lifts up to 20 kilograms while weighing only between four and 7.5 kilograms, depending on its size. This leaves the robot with enough payload for the actual handling task.The ZLW extends the SPZ series of layer gripping systems downwards and can grip several open, hollow or closed objects such as jars, cans or cardboard boxes with different dimensions simultaneously. It compensates for height differences in the workpiece layer with an optionally available spring-loaded flange. In addition, Schmalz configures the lightweight gripper individually: The user receives an efficient complete system with components that are matched to each other and to the task. The vacuum generator is also dimensioned so that it does not require more power than is necessary for process reliability. But this is not the only thing that increases the efficiency of the handling process: the new layer gripper also indirectly helps to keep the CO2 footprint low: Smaller robots require less power and thus support sustainable automation - for example in production feeding, automated warehousing or end-of-line palletizing.Schmalz has deliberately kept the design slim: The sealing element is optionally equipped with individual plug-in suction cups or a sealing foam. A frame connects these to the honeycomb plate, on which a pressure relief valve, the vacuum switch VSi and the flange are mounted. The vacuum generator stands separately.

Slovníček

Lifting Technology

With vacuum, workpieces can be lifted and placed or held at a specific position. More!Lifting technology is used in numerous automated and manual lifting operations in a wide range of industries.Lifting technology is one of the most important components in internal processes. Vacuum technology can be used to lift workpieces, deposit them at a specific position or hold them in a certain position. Schmalz offers a comprehensive range of lifting technology for both manual and automated processes. Schmalz successfully uses the vacuum medium to generate the lifting motion. Schmalz handling technology primarily consists of vacuum components vacuum gripping systems lifting devices.Lifting Technology for Use in Any ApplicationSchmalz has many years of expertise in the field of vacuum technology in numerous industries. Over the years, a variety of lifting equipment has been developed to meet the requirements of a specific sector, for example the glass or automotive industry.Lifting Technology for Automated Handling SystemsIn the area of automated handling, Schmalz gripping systems reduce cycle times and use intelligent technology to reduce operating costs. Vacuum technology for automated handling comprises the following systems at Schmalz: the area gripping systems FXP/FMP have enormous suction power and can handle even heavy workpieces quickly. The layer gripping system SPZ is particularly well-suited to use in warehouse and intralogistics applications: These grippers use a combination of vacuum technology together with a global vacuum and mechanical grippers, enabling entire product layers or pallets to be gripped. The vacuum suction spider SSP is configured as end-of-arm tooling to meet specific customer requirements and thus ensures the best possible lifting result. For pick and place applications with Delta, SCARA or articulated robots, Schmalz has developed a new lifting technology with the vacuum end effector VEE. The innovative modular system offers unique flexibility, since the number and position of vacuum suction cups can be adjusted. the innovative VEE technologys designed to safely handle high-speed applications.Lifting Technology for Manual Handling SystemsIn the field of manual lifting technology for heavy loads, Schmalz vacuum lifters,column-mounted jib cranes and crane systems are an ergonomic and fatigue-free solution. Even when handling lighter loads, the moving mass can amount to several tons during a single shift. Schmalz handling systems make manual handling processes efficient and ergonomic. At the same time, they consistently reduce operating costs thanks to a range of innovative functions. Having consultants on hand to provide advice and an individual system design also ensures that Schmalz lifting technology is perfectly adapted to customer-requirements. Schmalz makes a distinction between two types of vacuum technology for manual handling systems: the vacuum tube lifter Jumbo allows for ergonomic handling of loads weighing up to 300 kg with high switching precision. The vacuum lifter VacuMaster can be used to move loads weighing several tons safely and with health and safety in mind. Combined with Schmalz crane systems these devices offer ready-to-connect complete systems for your handling applications. Schmalz grippers are powerful tools in all areas of manual handling.

Úspěšný příběh

Automated Door Handling With Vacuum Suction Spider

This solution from Schmalz reduces employee workload, increases the degree of automation and improves process reliability at Josko. Details.Automated Door Handling With Vacuum Suction SpiderJosko, a renowned manufacturer of windows and doors, has worked with Schmalz to develop a highly automated solution for the efficient handling of heavy door panels. Thanks to an innovative suction spider and fully automatic robot integration, up to 80 door panels can be processed per day. This innovative solution reduces the strain on employees, increases the degree of automation and improves process reliability.WoodDoor leavesSuction SpidersAutomated handlingJosko Fenster und Türen GmbHThe door and window expert Josko was founded in 1960 as a one-man carpentry. In 2022, Josko generated a turnover of 215 million euros with over 1,000 employees. At its headquarters in Kopfing im Innkreis, Upper Austria, Josko today produces wood, plastics/aluminum and aluminum windows, house and interior doors on 39,000 square meters.Before the Schmalz solution was introduced, it was a challenge for Josko employees to move the heavy interior door panles. The door panels, which weighed up to 100 kilograms, could not be handled by one person alone, and handling them with two people was physically too strenuous. Although Josko already had manual handling solutions in place to handle this heavy work, there were no spare parts available for the ageing turning device on the sanding machine, so Josko was looking for an overall solution to reduce the workload and increase the level of automation in production at the same time.The new system is designed to reduce the workload on our specialists and increase the degree of automation.Instead of the old turning device on the sanding machine, Josko has introduced a new system consisting of two KUKA robots and the WEBER KSF sanding machine. The first robot picks up a door blank from the stack and places it on a conveyor belt in front of the sanding machine. The door leaf is fed through the machine to calibrate and sand the surface. The second robot then picks up the processed blank and places it on a rack. The first robot picks it up again, turns the door leaf and takes it back to the sanding machine to process the other half. The robots are circuitried with SPZ suction spiders from Schmalz, which ensure a safe grip of the door leaves. These suction spiders are specially tailored to Josko's requirements and are designed to provide optimum gripping surfaces for the door paneld while being light enough to enable fast movements. The suction spiders are based on the FMP-S gripping system with sealing foam. This gripping system is particularly suitable for heavy and rough workpieces and the sealing foam ensures a safe seal and a firm grip without damaging the workpiece. Vacuum generation takes place via a connector to the compressed air network and is controlled by valves. Thanks to the integrated system monitoring and sensor technology, the suction spiders operate with absolute process reliability. With the gripping solution from Schmalz, around 70 to 80 door panels are moved per day in an eight-hour shift, without the employees having to perform strenuous activities such as moving the heavy elements. The individual dimensions of the door panels can be easily selected via a display, which eliminates the need for manual programming and reduces potential sources of error. Overall, the Schmalz solution enables Josko to process the door panels efficiently and ergonomically, leading to an increase in productivity and employee satisfaction., , , , Automated door handling with the vacuum suction spider FMHDErgonomics, EfficiencyThe fully automated solutions relieve employees of strenuous manual tasks, Solution enables continuous operation with high production capacity

Slovníček

Grippers

Explanations of gripping technology for both manual & automated handling and vacuum clamping technology. More!Gripping systems from Schmalz are used in automated handling in a wide range of industries, such as packaging, wood or intra-logistics.Gripping systems are used in all areas of automated handling. Schmalz gripping technology is used, for example, in the handling of wood, packaging, cardboard boxes, in intra-logistics or in sheet metal processing. Gripping technology from Schmalz is operated with vacuum and is therefore called vacuum gripping systems. They are divided into four product categories: Area gripping systems, layer gripping systems, suction spiders and end effectors. Gripping technology from Schmalz is individually adapted to the customer's application and planned in collaboration with our Schmalz product experts.Grippers for automated handling systemsSchmalz has the largest range of vacuum technology on the market. Over 3500 different vacuum components can be used to create customized gripping solutions. The range includes a large number of vacuum suction cups for use in a variety of industries and applications. Schmalz also provides various special grippers using innovative gripping technology. These are ideal for special applications such as handling systems for solar wafers or textiles. A vacuum system also includes additional components, for example mounting elements vacuum generators valves filters as well as switches and system monitoring devices. Schmalz grippers reduce cycle times and optimize operating costs in the field of automated handling systems. The area gripping systems FXP/FMP possess enormous suction force. This allows them to handle even very heavy workpieces quickly. With its ingenious gripper, the layer gripping system SPZ is ideal for use in warehouse logistics and intra-logistics. By combining vacuum technology with a global vacuum and mechanical grippers, the system can grip entire product layers or pallets – even if they are not complete. The vacuum suction spider SSP offers end-of-arm tooling for a specific customer application, guaranteeing an optimal solution. With the vacuum end effector VEE Schmalz developed a new gripper specifically for pick and place applications using Delta, SCARA and articulated robots. The system offers exceptional flexibility. Thanks to the innovative modular system, the number and position of suction cups can be varied. The online configurator makes it extremely simple to design complete end effectors within just a few minutes. The innovative VEE technology is designed to safely handle high-speed applications with accelerations of up to 10 g.Grippers for manual handling systemsSchmalz vacuum lifters and crane systems are classified as manual handling systems. They are known for providing the optimum ergonomic, healthy working conditions. Even when handling lighter loads, the moving mass can amount to several tons during a single shift. Schmalz gripping systems make manual handling processes more efficient. At the same time, they reduce operating costs in the long term thanks to a number of innovative features. An extensive range of accessories plus a personalized consultation from our Schmalz systems consultants guarantees that Schmalz grippers will be perfectly configured to the requirements of the application. Schmalz makes a distinction between two types of vacuum technology for manual handling systems: the vacuum tube lifter Jumbo allows for ergonomic handling of loads weighing up to 300 kg with high switching precision. The vacuum lifting device VacuMaster can be used to move loads weighing several tons safely and with health and safety in mind. Combined with Schmalz crane systems these devices form read-to-connect complete systems for your handling tasks. Schmalz grippers are therefore powerful tools in all areas of manual handling.Grippers for clamping of workpiecesOne of the uses of grippers is clamping and holding workpieces in place during internal production processes. Schmalz provides clamping technology for all types of CNC machining centers. The innovative clamping technology from Schmalz is ideal for all CNC machining centers whether they are being equipped for the first time or they are being updated. Schmalz clamping technology therefore provides an economic alternative to investment in a new machine. Schmalz offers a number of different vacuum technology systems for CNC machining centers: The vacuum blocks for woodworking are ideal for efficient grid table, flat table and console table system setup. Innovative Innospann grippers significantly increase productivity during a renovation project.Additional information on Schmalz grippersClick here for further information about our extensive range of gripping systems:

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku