Schmalz

Pharmaceutical Industry

Scenario

Application

  • End-of-arm tooling within a fully automated production line in the pharmaceuticals industry

Task

  • Predictive maintenance and easy troubleshooting in difficult to reach areas
  • Easy access to service information from a smartphone using NFC

Solution

Schmalz' vacuum and pressure switch VSi is an ideal solution for fully automated production lines with complex tooling in difficult to reach areas. The electronic switches are modular in design, simple to integrate in the automation environment and visible throughout the entire process thanks to the use of innovative communication technology. The VSi from Schmalz represents a tremendous advancement for troubleshooting and maintenance tasks:

  • Device and process information is available in real time because the switch performs direct measurements during the process and communicates with the respective controllers via IO-Link
  • Device and process information can be parameterized and read out on a smartphone using NFC
  • Current vacuum or pressure level can be seen on the display and the status indicator (LED)

Customer Benefits

Maintenance procedures Without VSi [minutes] With VSi  [minutes] Benefits of VSi
Identifying the source/cause of an error and possible solutions 10 1 The VSi can prevent downtime: Real-time measurements are made available directly at the vacuum switch, in the controller via IO-Link or on a smartphone via NFC. The app suggests possible solutions 
Identifying the faulty product using status messages and user-specific localization 10 1 Various IO-Link parameters can be used to query the current switch status, the installation and storage location or the installation date
Adjusting settings 5 1 Operating instructions can be accessed using NFC; setting values can be copied directly from the switch, using NFC or via IO-Link control
Leakage measurement, energy monitoring and predictive maintenance - ✓  
       
Total 25 3

Potential Saving for a Bottling Machine in the Pharmaceuticals Industry

The user can enter and read out important process and device data in real-time via the controller, easily access service information and display detailed error descriptions on a mobile device. Just by reducing downtime and minimizing maintenance time − by an average of 22 minutes per day − yearly savings of up to EUR 30,000 can be achieved in the above scenario.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku