Muut tartuntatekniikat
- Erityiset tartuntatekniikat haastaville materiaaleille
- Turvallinen ja hellävarainen käsittely
Näytä luokka
Special grippers are used in applications in which regular suction cups cannot be used. Special grippers are used to handle wafers, films, paper, fragile workpieces or textile fiber composites. They serve as a connection element between the workpiece and the handling system just like the suction cup.
Schmalz separates special grippers into the following series:
Floating suction cups
Magnetic grippers
Needle grippers
Wafer grippers
Composite grippers
Thin glass gripper
Our selection aid includes information that should be observed when selecting the right special gripper.