Vacuum Filters
Filters are used to protect the vacuum generator or the valve in dusty environments. The filters are installed in the system between the suction cup and the vacuum generator or the valve.
Vacuum filters are often installed as central filters in the system. The vacuum filters have a degree of separation of almost 100%.
Vacuum cup filters are installed as decentralized filters directly in the vacuum line at the suction cup. Vacuum cup filters are used with light to medium contamination.
Inline filters are installed as decentralized filters directly in the vacuum line at the suction cup. Inline filters are used with small flows and light contamination.