Schmalz

High-performer for compressed air-free vacuum automation

With the Compact Pump GCPi, Schmalz presents a powerful vacuum generator with a purely electric suction and venting function. Supplemented by the electric 3/2-way compact valve LQE, the user receives a compressed air-free vacuum system with the performance of conventional ejector solutions.

The Compact-Pump GCPi is Schmalz' new all-electric vacuum generator.

All-electric vacuum systems are in demand wherever compressed air is not available and efficiency is the focus. This can be in manufacturing and assembly as well as in autonomous transport systems and robots. The new Compact Pump GCPi from J. Schmalz GmbH generates the vacuum required for handling with the help of an efficient double-head diaphragm pump. Instead of compressed air, it only needs a 24-volt supply, for example from a battery. Thanks to the integrated energy-saving control, the speed of the pump is controlled as needed and optimized for the respective workpiece.

Fast cycle with new compact valve

The GCPi is IoT-ready: Process parameters are entered via the integrated IO-Link interface or via digital control signals. In addition, it is possible to enter parameters via the LCD touch display attached to the device. The user reads out information about the process via the integrated NFC interface. Schmalz has equipped the GCPi with additional connections. The new LQE compact valve can also be operated via these: The all-electric 3/2-way valve has a very compact design and can be mounted directly on the gripper. This significantly accelerates evacuation and ventilation of the vacuum system. A sensor integrated in the LQE, which monitors the vacuum, ensures even greater process reliability. If independent suction circuits are to be implemented in the vacuum system, several LQE compact valves are used for decentralized control. The vacuum for this is generated - centrally - by the GCPi.

The Compact Pump GCPi is expected to be available from September 2022, and the Compact Valve LQE in the fourth quarter of 2022.

The electric Compact Pump GCPi handling cardboard boxes

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Izberite svoje podjetje Schmalz v eni od naslednjih regij:

Regije

Vaša regija ni na seznamu?

Schmalz ima mednarodno prodajno mrežo s prodajnimi partnerji v več kot 80 državah. Izberite jezik za našo mednarodno spletno stran.

URL, do katerega poskušate dostopati, ni v pravilnem jezikovnem ali državnem kontekstu.

Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico