Schmalz

New area gripper: Half portion with full power

With the FXP-60 and FMP-60, Schmalz is sending a slimmer series of its universal area gripper into the halls of glass and wood processors as well as intralogistics specialists. The new vacuum area gripping system is now available in various lengths and with or without an integrated vacuum generator.

The narrow area gripper handles workpieces regardless of their geometry, position and orientation.

J. Schmalz GmbH is slimming down its area gripper. In contrast to the established 130-millimeter-wide version, the FXP-60 and FMP-60 measure just 60 millimeters, making them ideal for use in tight spaces, with interfering contours or for single-beam handling. The slimness does not affect performance: an energy-efficient multi-stage ejector sits on top of the FXP-60, ensuring low running costs and high operational reliability. The FMP-60 variant is designed for an external vacuum generator.

Ideal areas of application are the automated handling of plastic, sheet metal, glass and wood as well as in intralogistics. Despite its narrow width, the FXP-/FMP-60 is not picky when it comes to the dimensions or pickup position of the workpiece. Thanks to integrated flow restrictor technology, the minimum degree of coverage is 50 percent. Thus, even workpieces with recesses or made of porous materials are no difficulty for the narrow gripper.

The new area gripper is particularly lightweight with its modular design consisting of an aluminum profile with sealing foam as the gripping surface. This enables high dynamics in the handling process. While the width is set, the customer can specify the length individually in 18-millimeter increments. The minimum is 316 millimeters for the FMP-60 variant and 388 millimeters for the version with integrated vacuum generator; the maximum is 1,972 millimeters.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.