Schmalz

Automated handling • Automotive • Metal sheets • Vacuum Suction Cups

Vacuum Suction Cups SAB within the Automotive Press Plant

Dynamic processing with cycle times which are as short as possible has to be ensured in an automotive pressing plant. The safe, precise handling of car body parts made of sheet aluminum was made possible by a vacuum suction cup from Schmalz. The video shows vacuum suction cups which were specially developed for handling automotive industry workpieces. SAB type vacuum suction cups are designed for dynamic handling of sheet metal and shorten cycle times. Deep drawing of sheet metal is prevented due to the large-scale, structured inner support.

SAB suction cups allow for absorption of high lateral forces even with oiled sheet metal. A special groove on the under side of the suction cup supports slide-free handling. Thanks to the design with 1.5 corrugations, the suction cup adjusts perfectly to curved workpieces, while the 1.5 corrugations simultaneously ensure excellent damping during attachment. SAB suction cups are used in feeder systems for press lines in the car industry, for example. In this application, vacuum suction cups of the type SAB are used. These suction cups are developed especially for the requirements of the automotive industry.

Show more
Product Inquiry

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart