Schmalz

The Guard of Vacuum and Pressure

Nothing gets past it. The volume flow sensor FS from Schmalz is located near the gripping point and reports volume flow deviations for both vacuum and pressure during the handling process. It thus monitors and optimizes processes.

The new volume flow sensor FS from Schmalz is ideal for monitoring vacuum and compressed air systems with small hose diameters.

With its new FS series, J. Schmalz GmbH has expanded its range of products with a robust and reliable sensor to monitor handling processes. Weighing just slightly more than a bar of chocolate, the compact measuring device can be easily attached to robot arms or gripper spiders. System integration is possible via an analog output and two adjustable switching points. The new vacuum component defines precise vacuum and pressure values from –0.9 to 8 bar and the volume flow between five and 200 liters per minute, even for thin hose diameters. If the defined threshold value is exceeded, the LCD display of the FS visually indicates this by changing color.

Applications for the sensor include the automated handling of car body parts, glass sheets, and food packaging. It recognizes when cereal packaging is incorrectly gripped or if there is leakage that affects efficiency. The display also provides an analysis of the cumulative compressed air consumption. The volume flow sensor FS allows operators to optimize processes at a reasonable cost.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku