Schmalz

FAQ - IO-Link

What is IO-Link?

IO-Link is a point-to-point communications standard for automation technology. IO-Link permits integrated communication at all levels, from sensors and actuators through superordinated controllers (PLCs) and beyond to the control level. An intelligent field device can transmit data about its status, energy consumption, and the process via this interface. At the same time, parameters of the controller may be modified and then transferred to the product.

How is a smart field device integrated into the system via IO-Link?

The intelligent field device is both supplied with power and integrated into the system via the IO-Link connection. The device is connected to the so-called IO-Link master via the IO-Link cable and from there is connected to the controller. This substantially reduces the cost of cabling in the system. Parameterization of the devices is saved in the superordinate automation system. If a field device is exchanged, the previous parameters can be transferred to it quickly via IO-Link.

The IO-Link master and the field device are connected by an unshielded three-core cable that is at most 20 meters long.

What is an IO-Link master?

A system can be comprised of multiple IO-Link devices. Each device is connected to the IO-Link master. The master provides the interface to the superordinate controller and controls the communication between connected IO-Link devices.

Where is the data stored?

The data can be stored in either external or company-internal clouds.

What is the difference between IO-Link and Ethernet?

IO-Link and Industrial Ethernet permit integrated communication at all levels, from sensors and actuators through superordinated controllers (PLCs) and beyond to the control level.

IO-Link is a point-to-point communication standard, while Ethernet is based on a bus system. Using Ethernet, multiple participants can communicate directly with each other. Unlike IO-Link, Ethernet does not need an additional IO-Link master for this purpose.

What is an IODD?

IODD stands for IO Device Description. It contains identification, process and device data for IO-Link interface-equipped sensors and actuators. The IODD consists of a main file and various image files.

Where can I find the IODD?

The IODD for each intelligent Schmalz device can be found in the online shop. First call up the item in question via its part number or designation. On the "Documentation" tab you'll find the IODD in addition to the operating instructions.

What is a function module?

Schmalz offers function modules for its intelligent devices with which the devices can be integrated into different control systems quickly and without requiring any major manual adaptations. Function modules for IO-Link devices simplify communications with the PLC by providing device and process parameters.

Where can I find function modules?

You can find corresponding function modules directly on the page of the product in the online shop. Call up the item in question via its part number or designation. On the "Documentation" tab you'll find the function modules in addition to the operating instructions.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku