Schmalz

FA-X / FA-M Error handling

DataDictionary Number (new) Error number
old
Text Display Possible cause Solution
130 0x0082 Bit 0 Internal error: data corruption Error 001 E01 Internal error: data corruption Supply voltage was disconnected too quickly after a parameter change; save process was not fully completed. Clear the error by restoring the factory setting with the [rE5] function or parameter. Use engineering tool to import a valid dataset. If the error [E01] occurs again after you reactivate the supply voltages, contact Schmalz Service.
130 0x0082 Bit 2 Supply voltage too low  Error 003 E07 Primary voltage too low Sensor supply voltage is too low. Check power supply unit and power load. Increase supply voltage
130 0x0082 Bit 3 Supply voltage too high  Error 004 E17 Primary voltage too high Sensor supply voltage is too high. Check power supply unit. Reduce supply voltage
130 0x0082 Bit 6 Short circuit at OUT2 Error 007   Short circuit at OUT2 Short circuit at OUT2. Check OUT2.
130 0x0082 Bit 10 Vacuum Sensor calibration failed Error 011 E03 Vacuum sensor calibration failed Zero-point adjustment for vacuum sensor is outside of the tolerance 3% FS. Calibration was canceled when measurement value was too high or too low. Vent the vacuum circuit. Calibrate the vacuum sensor again.
130 0x0082 Bit 11 Pressure Sensor calibration failed Error 012   Pressure sensor calibration failed Zero-point adjustment for pressure sensor is outside of the tolerance 3% FS. Calibration was canceled when measurement value was too high or too low. Vent the vacuum circuit. Calibrate the pressure sensor again.
130 0x0082 Bit 15 IO-Link communication interruption Error 016 E08 IO-Link communication abruption Connection to the master interrupted. Check connection line. Repeat the power-up process.
146 0x0092 Bit 0 Valve protection Warning 001   Valve protection active   Check the system for leakage. If necessary, adjust “Min. evacuation time” using the process settings.
146 0x0092 Bit 1 Evacuation time above limit Warning 002   Evacuation time above limit   Check the system for leakage. If necessary, adjust “Permissible evacuation time t1” using the process settings.
146 0x0092 Bit 2 Leakage rate above limitd Warning 003   Leakage above limit The set leakage rate was exceeded. Check the system for leakage. If necessary, adjust “Permissible leakage rate” using the process settings.
146 0x0092 Bit 3 SP1 not reached in suction cycle Warning 004   SP1 not reached in suction cycle The set switching point was not reached in the last cycle. Check the system for leakage. If necessary, adjust “SP1” using the process settings.
146 0x0092 Bit 4 Free Flow Vacuum over SP2 Warning 005   Free flow vacuum over SP2 During unobstructed suction, the vacuum value is above the parts detection level (SP2). Check the system for contamination and ensure that the cross sections are appropriate. If necessary, adjust SP2 using the process settings.
146 0x0092 Bit 5 Sypply voltage  out of operating range Warning 006   Primary voltage out of operating range Supply voltage: outside permissible range. Check the supply voltage.
146 0x0092 Bit 8 Input pressure out of operation range Warning 009   Input pressure out of operating range The input pressure is outside the specified range. Check the input pressure.
146 0x0092 Bit 12 Air saving function limited Warning 013   Air saving function limited, less vacuum detected The air-saving function detects a low vacuum and limits the minimum number of ejectors that can be deactivated. Check the system for leakage. If necessary, adjust “SP1,” “SP2” or “Min. evacuation time” using the process settings.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart