Schmalz

More Efficiency in Three Stages

Schmalz is equipping its compact ejector series SCPS(i) with three-stage ECO nozzle technology for the first time and making its vacuum generator even more powerful. The result is rapid handling processes with airtight, air-permeable or non-rigid workpieces such as particle boards, cardboard and bags. The optional IO-Link interface makes it easier to both monitor the vacuum level and use the technology in automated systems.

New ejector with efficient eco nozzle technology display and optional IO-Link technology. For use in dynamic processes with high flow rate requirements.

Combined with the compact ejectors SCPS/SCPSi, the eco nozzle technology provides a high suction rate with minimized compressed air consumption. Schmalz is offering ejectors with three-stage SEP modules for the first time: The new SCPS(i)-L series can now be used with a three-stage nozzle with a maximum diameter of 22 millimeters, which increases the application range of the ejector. The user can replace the SEP nozzles quickly without using tools – which also makes it easy to clean. The vacuum specialist also offers the ejector module separately.

Packaging system manufacturers in particular can reap the benefits of the new compact ejectors. The three installation diameters with different performance levels make the ejectors ideal for handling airtight or extremely air-permeable workpieces such as cardboard boxes or particle boards and even non-rigid workpieces such as bags. For airtight parts, Schmalz has lowered the evacuation time to reach 600 mbar – the time it takes to release the parts for travel for automation – by up to 10 percent. The SCPS(i)-L is deployed to provide vacuum power and monitoring in automated systems including robot handling applications, on linear axes and in pick-and-place applications with short cycle times. It is also ideal for dynamic gripping and fully automated parts handling. Device and process parameters can be applied and issued through the optional IO-Link interface. This feature is also available in SIO mode (standard IO).

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart