Automation Technology
In automation technology, artificial systems or “automats” are used to automate processes that were previously carried out manually. Individual machines or even entire industrial plants run a program independently and use this to make decisions about the control and regulation of the process. Humans are only indirectly involved in these control processes.
The more independent the complex machines are from human involvement, the higher the degree of automation. Advances in signal acquisition, electronic signal processing and intelligent products that collect process data and make it visible contribute to the expansion and efficient design of automation technology in many areas.
The aim was to have rigid, recurring production processes carried out as far as possible by machines and to achieve increases in productivity. However, the endeavors are now far more ambitious. Work sequences involving different tasks are undertaken by flexible production systems in order to achieve greater overall efficiency.
Automation technology is used, for example, in production processes in the automotive industry, handling and logistics processes.
Use of Vacuum Technology in Automation Technology
Vacuum technology can be used to automate many processes in a wide variety of industries. From individual components to entire systems, Schmalz offers products that further advance the automation and efficient, resource-saving design of production processes. In particular, the intelligent products (Smart Field Devices), such as the IO-Link-capable compact terminal SCTSi or the vacuum and pressure switch VSi, make process data transparent and enable predictive maintenance. Reducing downtime increases productivity in automation technology.
Prepared for the future – intelligent products for automation technology
Handling Process Data in Real Time
Schmalz develops smart field devices that enable process data to be used in real time. Our intelligent products feature integrated energy and process control functions. They collect and interpret data and then make it visible for the user.
One example is the compact terminal SCTMi. This compact terminal consists of up to 16 individual ejectors that can be controlled individually. A single compressed air supply and one electrical connection is all that is required. All relevant parameters, such as the energy consumption and performance in the vacuum system can be recorded, monitored and analyzed via the IO-Link interface.
Making Process Data Visible Using NFC Technology
In addition to an IO-Link interface, Schmalz provides an additional means of communication with intelligent products in the form of NFC technology. Process data is recorded directly and transferred securely to a smartphone via a point-to-point contact using NFC. Device and process information can also be parameterized on the smartphone.
Products
관련 용어
More Information

슈말츠 커넥트
빠른 통합, 완벽한 네트워크 구성, 지속적인 모니터링. 디지털 팩토리를 위한 슈말츠의 인더스트리 4.0 제품.

Smart Field Devices from Schmalz
Schmalz Connect combines the range of intelligent vacuum components, including vacuum generators, special grippers and vacuum and pressure switches. Choosing future-proof vacuum technology has never been so simple.
Schmalz Gripper in Action
Experience the Schmalz grippers in action in our media centre. Our experienced Schmalz system consultants will be happy to help you with the design of your vacuum system.