Schmalz

Pressure Switches

Electronic pressure switches are used in the measuring range from 0 to 10 bar. Pressure switches with digital display (VS-P10-D/ VS-P10-W-D) are easy to operate. The switching points and hysteresis are fully programmable using a foil keypad. They are used when there are high requirements for switching accuracy and repeatability as well as implementation of short switching times. Pressure switches with teach button (VS-P10AH/AV-T-PNP(-S)) are particularly suited to program switching points quickly and easily. Pressure switches with analog and digital output  (VS-P1 version) can also be used as pressure  sensors due to their two outputs.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.
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
Select 포트폴리오를 사용하면 전 세계에서 즉시 사용 가능하고 최적으로 조합할 수 있는 검증된 표준 제품을 신뢰할 수 있습니다. 더 이상 긴 납품 시간과 제품 선택의 불확실성이 없습니다. 빠르고 복잡하지 않으며 전 세계에서 사용 가능한 필요한 진공 부품을 정확하게 찾아보세요.