Schmalz

Vacuum Clamping Technology for the Fiber Composites Industry

Fiber-reinforced plastics are mainly reinforced by embedded glass fibers or carbon fibers. Carbon-fiber reinforced plastics (CFRP) have an even better ratio between strength and weight. This material is primarily used in the automotive, airline and wind energy industries, but is also used in sporting goods, construction and other sectors.

The last steps in processing give the workpiece its final shape. The workpieces must be held securely for processing in CNC machining centers or water jet cutting systems. These free-form surfaces are more difficult to process and present new challenges for clamping technology in particular.

Zapytanie o produkt
Wymagania

Requirements for Vacuum Technology

Clamping of workpieces during the finishing of composites components

  • In the final machining steps, the workpiece is given its final contour, for example, by trimming and drilling holes. For machining in CNC machining centers, the workpieces are securely fixed

  • Clamping with vacuum is used, for example, for joining and connecting processes (gluing, welding, soldering, etc.) in car body construction, the aerospace industry and in all sectors in which 3D free-form surfaces have to be gripped or fixed in place

  • Suitable for rigid workpieces - adjustable in z-, A- and C-axis (manual)

Positional accuracy and process reliability

  • An absolute prerequisite for functioning CFRP processes are gripping and clamping systems that operate with positional accuracy for handling and fixing three-dimensional components in manual or automated production processes

  • Free-form surfaces are correspondingly more complex to machine and pose new challenges, especially for clamping technology

Flexible setup of production lines with minimal downtimes

  • Flexibilization of production lines to reduce set-up times. Reduction of batch sizes for a more precise adjustment of the output quantity to the demand

  • Flexibility of the clamping device for small batch sizes with different contours are of great importance

  • Suitable for many common types of clamping tables

Automation in workpiece clamping

  • Software-controlled mapping of 3D free-form surfaces via a 2D reference surface creates the basis for automated setup processes for gripping and clamping systems

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adres URL, do którego próbujesz uzyskać dostęp, nie jest we właściwym języku lub kontekście kraju.

Kanał sklepu powiązany z Twoim kontem nie jest zgodny z kanałem żądanego adresu URL. Aby wyświetlić ceny lub złożyć zamówienie, przełącz się na kanał specyficzny dla użytkownika.

Produkt pomyślnie dodany do koszyka

Przejdź do koszyka

Schmalz Select - Preferowana gama produktów dla techniki podciśnieniowej

Wszystko dostępne. Wszystko ustawione. Wszystko jasne.

Dzięki portfolio Select można polegać na sprawdzonych, standardowych produktach, które są dostępne natychmiast i na całym świecie oraz mogą być optymalnie łączone. Koniec z długim czasem dostawy i niepewnością przy wyborze produktów. Znajdź dokładnie te części składowe, których potrzebujesz - szybko, nieskomplikowanie i dostępne na całym świecie.