Schmalz

Configuring spring plungers made easy

The FSTIm and FSTImc spring plungers can be individually adapted to different requirements. This provides companies with custom-made solutions for their plant automation. Schmalz offers a new online configurator with integrated error prevention to make the design process quick and easy.

Small or large, ESD-compatible or not - the FSTIm/FSTImc spring plungers can now be easily configured online.

Spring plungers in a small size have proven themselves in the electronics industry, in the pharmaceutical sector and in clean room applications: Thanks to the responsive spring, they handle very sensitive workpieces gently and offer particularly high positioning accuracy in combination with a flat suction gripper. The compact dimensions even fit into tight assembly lines. Due to the internal spring and the reduced tubing - especially with the profile version of the FSTImc - particle generation is reduced to a minimum. Additional effect: significantly shorter installation and maintenance times. And even surfaces with height tolerances are no problem for the small power packs. Thanks to the responsive movement and compact design of the FSTImc spring plunger in the cartridge design, delicate workpieces can be handled with process reliability.

The right spring plunger in just a few clicks

To speed up the design of automation systems and eliminate potential sources of error, Schmalz is launching a configurator for the FSTIm/FSTImc spring plungers. Designers and engineers save valuable time in development with the online tool. For example, they can not only choose between different plunger strokes, but also determine the type of vacuum connection, the version and the suction cup type or the threaded connection. The spring plungers support features such as ESD in the respective variants. The complete solution of spring plungers including mounting element and suction cups can be implemented in the planning after configuration via CAD model.

In contrast to the FSTE model (left), the spring in the FSTIm versions (center and right) is protected inside the housing.

Spring plungers handle components gently and make flexible pick-and-place applications possible.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.