Schmalz

Manual handling • Automotive • Car body parts • Vacuum tube lifters JumboErgo

Vacuum tube lifter JumboErgo for mark-free handling of panoramic roofs

An automotive supplier delivers panorama roofs weighing up to 30 kg to the OEMs. After being painted, these roofs are taken on a shelf truck to quality control. The panoramic roofs are inspected for quality defects, such as paint damage, on a holding device. In the past, this device was loaded and unloaded manually without the use of any lifting aids. The employees developed back problems as a result of constantly moving the roofs back and forth. To reduce the strain on staff and make the process more ergonomic, the company decided to invest in a vacuum lifter from Schmalz.

The vacuum tube lifter JumboErgo, with a maximum load of 35 kg, meets the requirement for this work step. The workpiece is lifted and deposited using solely the power of the vacuum. A powerful vacuum generator provides the necessary holding force. The operator is able to finely adjust the vacuum in the lift tube by means of a twist grip, which allows for optimum precision when moving the panoramic roofs. A venting unit integrated in the operating element allows easy removal of the air-tight workpiece. In order to prevent marks on the workpiece, the suction cups on the double gripper are fitted with suction cup covers.

The responsive column-mounted jib crane has a maximum load of 45 kg. The 6-meter long aluminum jib can swivel by up to 270 degrees, enabling it to cover a large working area. The column-mounted jib crane in combination with the tube lifter JumboErgo has made the process ergonomic and permanently taken the load off employees.
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.