Schmalz

Calculation of Evacuation Times

The entire volume that has to be evacuated is required to calculate the efficiency of the vacuum system.

VG = V1 + V2 + V3 + V4 + V5 + ...

VG = Volume to be evacuated [m3]
V1 = Volume of suction cups [m3]
V2 = Volume of mounting elements [m3]
V3 = Volume of vacuum hoses [m3]
V4 = Volume of distributor [m3]
V5 = Volume of prefilter (if necessary) [m3]
V6 = Volume of solenoid valve (if necessary) [m3]
...

Example:
VG = 6 x 35 cm3 + 6 x 9.5 cm3 + 6 x 43 cm3 + 1 x 38.5 cm3
VG = 564 cm3 = 0.000564 m3

Calculation of evacuation time t [h]

t = (VG x In (Pa/Pe) x 1,3)/V

VG = Volume to be evacuated [m3]
In = Natural logarithm
Pa = Absolute start pressure [1,013 mbar]
Pe = Absolute final pressure [mbar]
V = Suction rate of vacuum generator [m3/h]

Example:
t = (0.000564 m3 x In (1,013 mbar / *400 mbar) x 1.3) / 6.95 m3
t = 0,0000980 h = 0,35 sec

*60% = 400 mbar absolute
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.