Schmalz

Vacuum Pump for Mobile Robots

With the intelligent vacuum pump GSP, Schmalz is introducing an electric vacuum generator for mobile robotics applications and intralogistics processes. The demand-based pump control and automatic leakage detection adapt the power output to actual needs. As a result, energy consumption is reduced by up to 90 percent compared to conventional electric vacuum generators.

The intelligent control system detects whether the workpiece is airtight or porous and adapts the power output accordingly in real time. This can result in energy savings of up to 90 percent.

Autonomous mobile robots (AMRs) and automated guided vehicles (AGVs) have long since moved beyond mere transportation: They grasp, move, and handle objects on their own. Vacuum technology is key here: it combines gentle gripping with speed, flexibility, and reliability in dynamic processes.

Two technologies have become established in vacuum handling: electric vacuum generators, such as rotary vane or claw pumps, and pneumatic vacuum generators, known as ejectors. These are compact, lightweight, and suitable for dynamic processes. They require compressed air, which must be generated either centrally or locally. This requires two energy conversions: from electrical energy to compressed air and from compressed air to a vacuum. This makes the process energy-intensive.

Electric vacuum generators create a vacuum directly and do not require compressed air. However, many traditional solutions are large and heavy. Their mechanical parts also make them less dynamic, which means they should run as continuously as possible, even when a vacuum is not needed at times. Compact and energy-efficient solutions such as the ECBPMi and ECBPi vacuum generators, as well as the GCPi compact pump from Schmalz, partially bridge this gap. However, their maximum power of 50 liters per minute limits the range of applications, particularly in intra-logistic environments. Until now, there has been no solution for mobile and decentralized applications that provides a connection between a compact design, fast response, and high power.

Retrofitting without additional infrastructure

Schmalz addresses this need with the fully electric, ready to connect 24-V vacuum pump GSP. This pump enables automation solutions to be integrated flexibly into existing facility designs, independent of the compressed air network. This facilitates retrofitting and use in the automotive, glass, and packaging industries.

With a suction rate of 50 to 150 liters per minute, the intelligent vacuum pump GSP covers a wide range of applications. The vacuum pre-charge with the LQE compact valve and the integrated silencer reduce operating noise. In many cases, additional soundproofing measures are not necessary.

Up to 90 percent less energy consumption

At the heart of the vacuum pump is its intelligent control system. The speed automatically adapts to the actual vacuum level required. For airtight workpieces, the pump reduces its speed to zero and thus consumes virtually no energy. At the same time, it offers power reserves for fast cycles and for handling workpieces with leakage. Compared to conventional electric vacuum generators, the vacuum pump GSP saves up to 90 percent in energy. For mobile, battery-powered applications, this means significantly longer runtime or the ability to use smaller batteries.

Plug and play from the very first use

Designed for immediate use, the vacuum pump GSP is ready to operate right out of the box. No manual software setup is required. In combination with the LQE compact valve, Schmalz offers a plug-and-play solution in which the pump and valve communicate with each other autonomously. During the wait time between two gripping cycles, the system begins building up vacuum. At the next pick, the stored vacuum generates a targeted inflow pulse that accelerates the gripping process: This causes the workpiece to be drawn in more quickly. Atmospheric ventilation via the compact valve reduces energy consumption during workpiece release by up to 99 percent compared to conventional compressed-air blow-off methods. This interaction increases the possible cycle frequency and supports dynamic handling processes in order fulfillment and intra-logistic operations.

Automatic Start of Operations and Diagnostics

The NFC interface simplifies start of operations and diagnostics through smartphone access. Process and device data can be viewed at any time on the integrated color display and are transmitted to the higher-level PLC during IO-Link operation. The pump automatically detects whether it is connected to an IO-Link master and switches to the appropriate mode on its own. Using the transmitted vacuum values and diagnostic information, the system identifies potential malfunctions early on. Alternatively, the pump can also be controlled via standard I/O. The pump automatically determines the material porosity of the workpiece being handled—whether cardboard box, plastics, or metal—and adapts the flow rate accordingly.

Process reliability even during a power outage

The vacuum pump GSP automatically detects leakage as it occurs and adjusts the pump capacity without requiring any user intervention. Optionally, it can be designed for an uninterruptible power supply (UPS). This ensures that air-tight workpieces are held in place for up to 20 hours, even in the event of a power or grid failure.

Robot-to-Goods processes enable autonomous order picking that does not require a central compressed air system. Autonomous robots retrieve orders from the storage facility on their own. The vacuum pump GSP is particularly compact, lightweight, and energy-efficient, which extends battery life.

The vacuum generator is suitable for applications requiring low levels of compressed air, such as loading and unloading sheet metal parts in preform presses and joining machines, as well as for material handling in intra-logistic operations.

When combined with the LQE electrical compact valve, Schmalz creates a perfectly coordinated system. It enables exceptionally fast pickup and set-down times, up to 99% less energy consumption when setting down parts compared to conventional methods, and significantly lower noise levels.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Các công ty Schmalz

Vui lòng chọn công ty Schmalz tại một trong các khu vực sau:

Các khu vực

Khu vực của bạn không có trong danh sách?

Schmalz duy trì một mạng lưới bán hàng quốc tế với các đối tác phân phối tại hơn 80 quốc gia. Vui lòng chọn ngôn ngữ cho trang web quốc tế của chúng tôi.

URL được truy cập không nằm trong bối cảnh ngôn ngữ-quốc gia phù hợp

Kênh cửa hàng được xác định dựa trên tài khoản người dùng của bạn không trùng khớp với kênh của URL đang được truy cập. Để xem giá hoặc đặt hàng, vui lòng chuyển sang kênh dành riêng cho người dùng của bạn.

0 Sản phẩm đã được thêm vào giỏ hàng thành công

Đến giỏ hàng