Schmalz

JumboFlex 50 – New Suction Plate for Handling Cardboard Boxes

Schmalz has added an oval suction plate with a size of 180x90 to its SAOF series. Up to this point, the only gripper solutions available were for the JumboFlex series 20 and 35, with a maximum lift capacity of 20 and 35 kg respectively. The new size means it can also now be combined with the vacuum tube lifters JumboFlex and JumboFlex High-Stack for workpieces weighing up to 50 kg. This new arrival adds another gripper to Schmalz’s JumboFlex modular system. In combination with the new beams, it allows the user to configure double or even four-head suction grippers to optimally meet his or her requirements.

Handling unstable cardboard boxes using a vacuum tube lifter JumboFlex with double suction grippers made up of two new suction plates SAOF 180x90.

Elongated suction plates offer an alternative to round suction cups. They are primarily used in intra-logistics, where unstable cardboard or slightly curved parts need to be lifted securely and gently. The suction plates in the SAOF series are made from wear-resistant nitrile rubber (NBR) and are ideal for the workpiece surfaces to be handled. The SAOF also now comes in a size with dimensions of 180 mm x 90 mm. J. Schmalz GmbH gave the suction plate adequate dimensions to ensure it remains compact but still has the suction area required for the vacuum tube lifter JumboFlex 50. That means it can safely transport loads of up to 50 kilograms. Along with this addition to the SAOF range, Schmalz has also introduced new grippers to the JumboFlex portfolio that allow it to cater for even more specific customer requirements. The following double suction gripper versions are available for the JumboFlex series 20, 35 and 50: with adjustable or non-adjustable suction plates, with beams in standard dimensions or in custom lengths. The grippers have a compact design and are also suitable for smaller workpieces. 

Schmalz is also introducing new beams for the new grippers. These beams can be used to connect up to four suction plates of your choice. Since the position of both the suction plates and the cross beams can be adjusted, the user can find the perfect gripper for every workpiece size. 

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku