Schmalz

Ruční manipulace • Dřevo • Dveře • Vakuové zvedáky trubek JumboErgo

JumboErgo Vacuum Tube Lifter for Efficiently Loading CNC Machining Centers

A Swiss door manufacturer has specialized in the production of wooden doors. The raw material is processed with a CNC machining center. The loading of this machine with the heavy wooden beams was previously done by two employees by hand. In order to protect the health of the employees and to organize the process ergonomically and efficiently, the company decided to purchase a vacuum tube lifter from Schmalz.

The JumboErgo vacuum tube lifter is designed for the effortless handling of wood panels weighing up to 65 kg. The ergonomic control handle allows the operator to raise and lower the workpiece in an intuitive turning motion. The lifting tube is equipped with a surface gripper which is specially designed for rough surfaces. The gripper can be positioned flexibly on the workpiece because a high gripping force is achieved due to the good sealing of the foam.

The lifting tube is supplemented by a Schmalz soft aluminum rolling beam.

Zobrazit více
Product Inquiry

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku