Schmalz

Schmalz: New liquid separator keeps every pump dry

Anyone who clamps with vacuum during CNC machining must protect the pump from cooling lubricant. The new NLS liquid separator from Schmalz separates the cooling lubricant and returns it to the running process - without interrupting the vacuum.

The compact NLS liquid separator from Schmalz is sure to keep any vacuum pump dry.

Vacuum clamps with low distortion and enables machining from five sides in one clamping. It becomes challenging when cooling lubricants are used: If these get into the vacuum generator, they cause serious damage. Schmalz has developed the NLS liquid separator to reliably separate suctioned liquid, dirt and chips beforehand. Located between the pump and the clamping device, it is integrated into the machine control system via a network module. This means that the operator can operate the NLS directly and conveniently via the HMI module of the milling machine.

The new Schmalz solution works with two chambers. There is a permanent vacuum in the upper chamber. The valve to the lower chamber is open from the start and the liquid collects there. When the lower chamber is full, the valve is closed by overpressure and the lower chamber is emptied. This allows the collected cooling lubricant to automatically return to the machine process via a hose.

The system permanently monitors the fill level and - with the help of a digital switch with IO-Link function - the vacuum, thus ensuring safe clamping during machining. In this way, the NLS ensures that the pump can constantly generate and maintain a high vacuum level in the system, even during running times of several hours or days.

The NLS is the successor to the VOC vacuum operation center. Compared to the latter, it is significantly more compact and less expensive. It is compatible with any Schmalz pump and is suitable for the initial equipment of CNC processing machines with vacuum supply. The product is ideally suited for OEMs and machine manufacturers.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart