Schmalz Calculator
The Schmalz Calculator is a powerful tool for calculating the characteristics of a vacuum system. This useful application is available free of charge as a Progressive Web App (PWA) and can be easily installed on computers and mobile devices. This means that the full functionality of the calculator is available even without an internet connection.
With the Schmalz Calculator, users can quickly and accurately calculate important values for their vacuum system. These include the required number of suction cups, the ideal suction cup diameter, the suction force needed to handle a workpiece and the optimum hose distribution. By entering the appropriate parameters, the Schmalz Calculator provides immediate results, enabling efficient evaluation and optimization of the vacuum system.
The application is characterized by its user-friendly interface, which allows easy entry of the required parameters. With just a few clicks, users get instant results and can design their vacuum systems quickly and easily.
Whether in industry, mechanical engineering or other technical applications, the Schmalz Calculator is an indispensable tool for professionals working with vacuum systems. Whether in the office, in the workshop or on the road, the Schmalz Calculator is the ideal tool for efficiently analyzing and optimizing vacuum systems.
Use the Schmalz Calculator now to help you design your vacuum system:
With the Schmalz Calculator you get information about:
- Required number of suction cups
- Suction area and cup diameter
- Required suction force
- Required theoretical holding force
- Ideal hose distribution
- Evacuation time
- Suction rate for pumps
- Hose diameter
Schmalz's expertise in vacuum technology and many years of experience in the field of system design are also the basis for the development of the Schmalz Calculator. It is hardly possible to determine values in the vacuum range more quickly and safely.