Vacuum Lifting Devices VacuMaster Basic
- For lift capacities up to 750 kg
- Ergonomic operator handle
- Malfunction-free manual sliding valve with clamp-safe catch lever
Their production of natural cosmetics involves the storage of essential oils in barrels. These barrels are delivered on wooden pallets, but must be transferred to aluminum pallets due to high purity requirements. Since each barrel weighs approximately 200 kg, this process demanded an enormous amount of physical effort on the part of the employees.
The vacuum lifting device VacuMaster Basic can lift one barrel at a time with ease. The electronic warning device of the lifting device provides protection for the employee in the event of a power failure. In such a case, the vacuum reservoir ensures a safe holding of the barrel. Because the operator handle is easy to reach, the lifting device is especially ergonomic and provides the required degree of protection of the employees’ health. In combination with a monorail that is attached to the wall, the lifting device can be used optimally in this area.
Discover application examples of the product in various industries - user-friendly, informative and practical.
No suitable videos found? Then take a look at our media center.