Vacuum Lifting Devices VacuMaster Window 200/300
- VacuMaster Window for vertical handling of windows, glass sheets and glass components
- Workpieces can be rotated to the side by 90°, with optional electric drive
- For lift capacities up to 300 kg
The firm uses a glass-cleaning system to clean glass sheets prior to insertion and installation into wooden frames. Up to 150 sheets are cleaned daily with the cleaning system. Previously, two employees were required to handle the glass sheets. A vacuum lifting device is now used to make the process easier and more efficient.
With the vacuum lifting device VacuMaster Window, glass plates weighing 170 kg are easily lifted off the glass trolley and deposited on the cleaning system. Surface scratches are prevented through the use of two SPU suction plates. VacuMaster Window is extremely easy to use, and because it was designed according to the latest ergonomic findings, the work can now be performed without endangering the employees’ health. The glass plates can be rotated 90° to the left and right so that they can be placed onto the cleaning system in the proper position according to their format. Only one employee is required to operate the VacuMaster Window.
Discover application examples of the product in various industries - user-friendly, informative and practical.
No suitable videos found? Then take a look at our media center.