Schmalz

Vacuum lifter packages

Vacuum lifters for parcels are the name given to Schmalz devices in the field of handling that use vacuum to safely and quickly transport a large number of letters, packages, parcels, all the way to bulky or particularly sensitive goods. The vacuum tube lifter JumboFlex is perfectly suited for parcel handling.

Short throughput times are required in logistics centers. As a result, the number of lifting tasks performed by employees is increasing. With the vacuum tube lifter Jumbo, the power-consuming lifting, rotating and moving is made easier by vacuum.

Etsi yhteyshenkilösi

The vacuum tube lifters JumboFlex

Increased handling speeds in postal centers or logistics hubs of other service providers require fast handling of a wide variety of handling tasks. With the vacuum tube lifter JumboFlex, you can move lighter goods weighing up to 50 kg ergonomically and at high cycle frequency. Its one-handed control handle fits comfortably in the hand and enables long, fatigue-free working. The quick-change system allows you to change suction cups quickly. Another feature is that laterally suctioned workpieces automatically swivel back to the horizontal and can be continuously rotated in this position. The employee is relieved of the weight of the workpieces by the vacuum tube lifter and can thus ergonomically realize the required handling frequency.

Products

The right crane system from Schmalz for every vacuum lifter for packages

The Schmalz modular system enables perfect integration of the vacuum tube lifter into your working environment. The vacuum lifter for packages from Schmalz is completed with a crane system that is precisely adapted to your application.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

URL-osoite, jota yrität käyttää, ei ole oikeassa kieli- tai maakontekstissa.

Tiliin liittyvä myymälän kanava ei vastaa pyydetyn URL-osoitteen kanavaa. Jos haluat tarkastella hintoja tai tehdä tilauksen, vaihda käyttäjäkohtaiseen kanavaan.

0 tuotteet lisätty onnistuneesti ostoskoriin

Mene ostoskoriin

Schmalz Select - Suositeltava tuotevalikoima alipainetegnologiaan

Kaikki saatavilla. Kaikki valmiina. Kaikki selvää.

Select-valikoiman avulla voit luottaa hyväksi todettuihin vakiotuotteisiin, jotka ovat välittömästi ja maailmanlaajuisesti saatavilla ja joita voidaan yhdistellä optimaalisesti. Ei enää pitkiä toimitusaikoja ja epävarmuutta tuotteiden valinnassa. Löydät juuri tarvitsemasi komponentit - nopeasti, mutkattomasti ja maailmanlaajuisesti saatavilla.