Schmalz

Vacuum lifter packages

Vacuum lifters for parcels are the name given to Schmalz devices in the field of handling that use vacuum to safely and quickly transport a large number of letters, packages, parcels, all the way to bulky or particularly sensitive goods. The vacuum tube lifter JumboFlex is perfectly suited for parcel handling.

Short throughput times are required in logistics centers. As a result, the number of lifting tasks performed by employees is increasing. With the vacuum tube lifter Jumbo, the power-consuming lifting, rotating and moving is made easier by vacuum.

연락처 찾기

The vacuum tube lifters JumboFlex

Increased handling speeds in postal centers or logistics hubs of other service providers require fast handling of a wide variety of handling tasks. With the vacuum tube lifter JumboFlex, you can move lighter goods weighing up to 50 kg ergonomically and at high cycle frequency. Its one-handed control handle fits comfortably in the hand and enables long, fatigue-free working. The quick-change system allows you to change suction cups quickly. Another feature is that laterally suctioned workpieces automatically swivel back to the horizontal and can be continuously rotated in this position. The employee is relieved of the weight of the workpieces by the vacuum tube lifter and can thus ergonomically realize the required handling frequency.

Products

The right crane system from Schmalz for every vacuum lifter for packages

The Schmalz modular system enables perfect integration of the vacuum tube lifter into your working environment. The vacuum lifter for packages from Schmalz is completed with a crane system that is precisely adapted to your application.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

액세스하려는 URL이 올바른 언어 또는 국가 컨텍스트에 맞지 않습니다.

계정에 연결된 스토어 채널이 요청된 URL의 채널과 일치하지 않습니다. 가격을 확인하거나 주문하려면 사용자별 채널로 전환하세요.

0 장바구니에 제품이 성공적으로 추가되었습니다.

장바구니로 이동