Schmalz

Vacuum Pump

Vacuum pumps are used to generate a vacuum. There are three different basic types of pump at Schmalz, and these are available in different sizes. These vacuum generators have a high suction rate, which enables them to handle porous and air-permeable workpieces. This makes them a crucial element for lifting and transporting objects of all kinds with a vacuum.

Functional Principle of Vacuum Pumps

A vacuum pump contains a ribbed impeller that is mounted eccentrically. The ribs in the pump are pressed outward by the centrifugal force, creating chambers of different sizes. These chambers are sealed by the ribs. The rotation causes the chambers to enlarge and the air to expand. The air pressure in the vacuum generator therefore decreases, producing a vacuum. During this process, the air is sucked out on the suction side of the vacuum generator. The compressed air (exhaust air) exits through the outlet opening of the pump.

The considerable compression of vacuum pumps enables them to generate a very high vacuum and means they have a relatively high suction rate depending on the type.

Advantages of Vacuum Pumps:

  • High vacuum level with high evacuation volume

  • Centralized vacuum generation with pumps

Typical Areas of Application:

  • Vacuum pumps are used for centralized vacuum generation in gantry transfer systems

  • In manual vacuum handling systems

  • In packaging machines

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

URL-osoite, jota yrität käyttää, ei ole oikeassa kieli- tai maakontekstissa.

Tiliin liittyvä myymälän kanava ei vastaa pyydetyn URL-osoitteen kanavaa. Jos haluat tarkastella hintoja tai tehdä tilauksen, vaihda käyttäjäkohtaiseen kanavaan.

0 tuotteet lisätty onnistuneesti ostoskoriin

Mene ostoskoriin

Schmalz Select - Suositeltava tuotevalikoima alipainetegnologiaan

Kaikki saatavilla. Kaikki valmiina. Kaikki selvää.

Select-valikoiman avulla voit luottaa hyväksi todettuihin vakiotuotteisiin, jotka ovat välittömästi ja maailmanlaajuisesti saatavilla ja joita voidaan yhdistellä optimaalisesti. Ei enää pitkiä toimitusaikoja ja epävarmuutta tuotteiden valinnassa. Löydät juuri tarvitsemasi komponentit - nopeasti, mutkattomasti ja maailmanlaajuisesti saatavilla.