Schmalz

Vacuum Pump

Vacuum pumps are used to generate a vacuum. There are three different basic types of pump at Schmalz, and these are available in different sizes. These vacuum generators have a high suction rate, which enables them to handle porous and air-permeable workpieces. This makes them a crucial element for lifting and transporting objects of all kinds with a vacuum.

Functional Principle of Vacuum Pumps

A vacuum pump contains a ribbed impeller that is mounted eccentrically. The ribs in the pump are pressed outward by the centrifugal force, creating chambers of different sizes. These chambers are sealed by the ribs. The rotation causes the chambers to enlarge and the air to expand. The air pressure in the vacuum generator therefore decreases, producing a vacuum. During this process, the air is sucked out on the suction side of the vacuum generator. The compressed air (exhaust air) exits through the outlet opening of the pump.

The considerable compression of vacuum pumps enables them to generate a very high vacuum and means they have a relatively high suction rate depending on the type.

Advantages of Vacuum Pumps:

  • High vacuum level with high evacuation volume
  • Centralized vacuum generation with pumps

Typical Areas of Application:

  • Vacuum pumps are used for centralized vacuum generation in gantry transfer systems
  • In manual vacuum handling systems
  • In packaging machines

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen