Schmalz

Vacuum Suction Cup

Vacuum suction cups come in a wide range of shapes, sizes and materials. The suction cups act as the connecting element between the machine and workpiece, and are used to lift and transport objects of all kinds.

Suction Cups Connect the Workpiece and System

Suction cups form the interface to the workpiece and thus play a major role in vacuum systems. To grip the workpiece securely, the suction cups must be suited to the workpiece properties and the particular application. For example, resistance to high temperatures, oils, dirt or UV light may be required. If the suction cups are to be used in the food industry, other properties must be taken into account.

Schmalz develops suction cups specially tailored to the requirements of the various industries, including the automotive, packaging and glass industries.

A vacuum suction cup consists of two components: the suction cup (elastomer section) and the corresponding connection element. A suction cup can be screwed to the gripper of the vacuum system.

Different Suction Cup Shapes

Suction cups are available in round and oval designs. Round suction cups are particularly suitable for handling flat workpieces. In contrast, oval suction cups are primarily used for handling narrow, elongated workpieces.

A distinction is also made between flat suction grippers and bellows suction cups.

Flat Suction Gripper

Flat suction grippers have a low overall height and low internal volume. The low volume ensures short blow-off times. In addition, suction cups in this design have good intrinsic stability and ensure high positioning accuracy. Frequent applications of flat suction grippers are mainly highly dynamic processes.

Bellows Suction Cup

Suction cups with one or more folds are extremely versatile. The fact that bellows suction cups feature one or more folds allows them to compensate for height differences, making them more flexible to use than flat suction cups. The folds also create a damping effect when the gripper is placed on the workpiece. This enables sensitive workpieces to be gripped gently. Bellows suction cups are often used for handling processes involving film-packed workpieces, car body parts or electronic components.

Products

Aiheeseen liittyvät termit

Bellows-type Suction Cup
Bellows suction cups are vacuum cups with one or more bellows. Due to the bellows, they enable particularly gentle handling of the workpiece.
Flat Suction Cups
Flat vacuums are vacuums in a flat design, with a small internal volume.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

URL-osoite, jota yrität käyttää, ei ole oikeassa kieli- tai maakontekstissa.

Tiliin liittyvä myymälän kanava ei vastaa pyydetyn URL-osoitteen kanavaa. Jos haluat tarkastella hintoja tai tehdä tilauksen, vaihda käyttäjäkohtaiseen kanavaan.

0 tuotteet lisätty onnistuneesti ostoskoriin

Mene ostoskoriin

Schmalz Select - Suositeltava tuotevalikoima alipainetegnologiaan

Kaikki saatavilla. Kaikki valmiina. Kaikki selvää.

Select-valikoiman avulla voit luottaa hyväksi todettuihin vakiotuotteisiin, jotka ovat välittömästi ja maailmanlaajuisesti saatavilla ja joita voidaan yhdistellä optimaalisesti. Ei enää pitkiä toimitusaikoja ja epävarmuutta tuotteiden valinnassa. Löydät juuri tarvitsemasi komponentit - nopeasti, mutkattomasti ja maailmanlaajuisesti saatavilla.