Schmalz

Bellows-type Suction Cup

Bellows suction cups consist of vacuum suction cups (elastomer part) with one or more folds. Bellows suction cups are available in an oval or round designs. In addition to bellows suction cups, Schmalz offers a wide range of flat suction cups.

The bellows suction cup acts as a connection piece between the handling system and the workpiece

Bellows suction cups are selected based on their bellows. Thanks to the bellows, the vacuum suction cup can be positioned on the workplace extremely gently. The bellows suction cup cushions the vacuum system, which protects the workpiece. The bellows also make the suction cup particularly flexible and adaptable. In addition, some inaccuracies such as height differences or unevenness can be easily compensated with the bellows suction cup.

As soon as the bellows suction cup is placed on the workpiece, the sealing lip seals the vacuum suction cup. The air can then be sucked out of the vacuum suction cup. The bellows suction cup contracts and the workpiece is lifted (lifting effect). This effect is used, for example, when a workpiece has to be lifted out of a mold or stacked using a suction cup.

Bellows suction cups are often used in packaging processes. These vacuum suction cups are suitable for handling non-rigid workpieces such as products packaged in film. However, electronic components are also handled with bellows suction cups. The gentle damping effect is particularly useful in this application. Compensating for heights and careful handling is required when moving uneven car body parts or pipes and cardboard boxes.

Vacuum grippers are either inserted directly into the gripping system or screwed into the gripping system using a connection element. Together with the connection element, the bellows suction cup (elastomer part) becomes a bellows vacuum gripper.

Products

Aiheeseen liittyvät termit

Vacuum Suction Cup
Vacuum cups connect the workpiece and the system and are available in various shapes.
Flat Suction Cups
Flat vacuums are vacuums in a flat design, with a small internal volume.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

URL-osoite, jota yrität käyttää, ei ole oikeassa kieli- tai maakontekstissa.

Tiliin liittyvä myymälän kanava ei vastaa pyydetyn URL-osoitteen kanavaa. Jos haluat tarkastella hintoja tai tehdä tilauksen, vaihda käyttäjäkohtaiseen kanavaan.

0 tuotteet lisätty onnistuneesti ostoskoriin

Mene ostoskoriin

Schmalz Select - Suositeltava tuotevalikoima alipainetegnologiaan

Kaikki saatavilla. Kaikki valmiina. Kaikki selvää.

Select-valikoiman avulla voit luottaa hyväksi todettuihin vakiotuotteisiin, jotka ovat välittömästi ja maailmanlaajuisesti saatavilla ja joita voidaan yhdistellä optimaalisesti. Ei enää pitkiä toimitusaikoja ja epävarmuutta tuotteiden valinnassa. Löydät juuri tarvitsemasi komponentit - nopeasti, mutkattomasti ja maailmanlaajuisesti saatavilla.