Schmalz

Bellows-type Suction Cup

Bellows suction cups consist of vacuum suction cups (elastomer part) with one or more folds. Bellows suction cups are available in an oval or round designs. In addition to bellows suction cups, Schmalz offers a wide range of flat suction cups.

The bellows suction cup acts as a connection piece between the handling system and the workpiece

Bellows suction cups are selected based on their bellows. Thanks to the bellows, the vacuum suction cup can be positioned on the workplace extremely gently. The bellows suction cup cushions the vacuum system, which protects the workpiece. The bellows also make the suction cup particularly flexible and adaptable. In addition, some inaccuracies such as height differences or unevenness can be easily compensated with the bellows suction cup.

As soon as the bellows suction cup is placed on the workpiece, the sealing lip seals the vacuum suction cup. The air can then be sucked out of the vacuum suction cup. The bellows suction cup contracts and the workpiece is lifted (lifting effect). This effect is used, for example, when a workpiece has to be lifted out of a mold or stacked using a suction cup.

Bellows suction cups are often used in packaging processes. These vacuum suction cups are suitable for handling non-rigid workpieces such as products packaged in film. However, electronic components are also handled with bellows suction cups. The gentle damping effect is particularly useful in this application. Compensating for heights and careful handling is required when moving uneven car body parts or pipes and cardboard boxes.

Vacuum grippers are either inserted directly into the gripping system or screwed into the gripping system using a connection element. Together with the connection element, the bellows suction cup (elastomer part) becomes a bellows vacuum gripper.

Products

관련 용어

Flat Suction Cups
Flat vacuums are vacuums in a flat design, with a small internal volume.
Vacuum Suction Cup
Vacuum cups connect the workpiece and the system and are available in various shapes.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

액세스하려는 URL이 올바른 언어 또는 국가 컨텍스트에 맞지 않습니다.

계정에 연결된 스토어 채널이 요청된 URL의 채널과 일치하지 않습니다. 가격을 확인하거나 주문하려면 사용자별 채널로 전환하세요.

0 장바구니에 제품이 성공적으로 추가되었습니다.

장바구니로 이동