Schmalz

Bellows-type Suction Cup

Bellows suction cups consist of vacuum suction cups (elastomer part) with one or more folds. Bellows suction cups are available in an oval or round designs. In addition to bellows suction cups, Schmalz offers a wide range of flat suction cups.

The bellows suction cup acts as a connection piece between the handling system and the workpiece

Bellows suction cups are selected based on their bellows. Thanks to the bellows, the vacuum suction cup can be positioned on the workplace extremely gently. The bellows suction cup cushions the vacuum system, which protects the workpiece. The bellows also make the suction cup particularly flexible and adaptable. In addition, some inaccuracies such as height differences or unevenness can be easily compensated with the bellows suction cup.

As soon as the bellows suction cup is placed on the workpiece, the sealing lip seals the vacuum suction cup. The air can then be sucked out of the vacuum suction cup. The bellows suction cup contracts and the workpiece is lifted (lifting effect). This effect is used, for example, when a workpiece has to be lifted out of a mold or stacked using a suction cup.

Bellows suction cups are often used in packaging processes. These vacuum suction cups are suitable for handling non-rigid workpieces such as products packaged in film. However, electronic components are also handled with bellows suction cups. The gentle damping effect is particularly useful in this application. Compensating for heights and careful handling is required when moving uneven car body parts or pipes and cardboard boxes.

Vacuum grippers are either inserted directly into the gripping system or screwed into the gripping system using a connection element. Together with the connection element, the bellows suction cup (elastomer part) becomes a bellows vacuum gripper.

Products

Verwante termen

Vacuum Suction Cup
Vacuum cups connect the workpiece and the system and are available in various shapes.
Flat Suction Cups
Flat vacuums are vacuums in a flat design, with a small internal volume.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.