Schmalz

Vacuum Lifter Natural Stone

Vacuum lifters for natural stone are devices in materials handling that are able to lift, move and deposit heavy and unwieldy natural stone with the help of a vacuum. The vacuum tube lifter Jumbo can be used for this application:

  • Vacuum Tube Lifter JumboErgo
  • Vacuum Tube Lifter JumboSprint

Ergonomics and increased efficiency are among the most important features of vacuum lifters for natural stone from Schmalz. As a result, you can reduce or avoid absences due to illness and thus increase productivity.

연락처 찾기

Options for Handling Natural Stone

You can ergonomically move natural stone weighing up to 300 kg with the two vacuum tube lifters JumboErgo and JumboSprint. The vacuum tube lifter JumboErgo is ideal for workpieces with different formats. The vacuum tube lifter JumboSprint is ideal when using compact workpieces.

Schmalz Products for Handling Natural Stone

Discover the perfect vacuum lifter for handling natural stone:

Products

The Right Schmalz Crane System for Every Vacuum Lifter for Natural Stone

The Schmalz modular system allows the vacuum tube lifter to be perfectly integrated into your working environment. The Schmalz vacuum lifter for natural stone is enhanced with a crane system that is precisely tailored to your application.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

액세스하려는 URL이 올바른 언어 또는 국가 컨텍스트에 맞지 않습니다.

계정에 연결된 스토어 채널이 요청된 URL의 채널과 일치하지 않습니다. 가격을 확인하거나 주문하려면 사용자별 채널로 전환하세요.

0 장바구니에 제품이 성공적으로 추가되었습니다.

장바구니로 이동