Schmalz

Selection Aid for Filters And Connectors

Overview Flow Resistance In Hoses

Aid for the dimensioning of distribution hoses:
Example: A hose with an internal diameter D = 32 mm has the same internal flow rate as 32 hoses with an internal diameter of 6 mm or 4 hoses with an internal diameter of 16 mm.

Checklist For Selection Of Hoses

Criterion/Material PVC PU PE PA
Resistance to oil Good Excellent Good Very good
Resistance to fuels and natural gas Medium Very good Medium Good
Resistance to weathering Medium Excellent Medium Medium
Behaviour at low temperatures Freezes at -20°C Similar to a hard plastic at -35° bis
-40°C, but no embrittlement
Freezes at -50°C Freezes at -40°C
Behaviour at high temperatures Withstands 70°C for long periods Withstands 80°C for long periods, for short periods up to 100° Withstands 70°C for long periods Withstands 85°C for long periods
Dynamic stress resistance Tensible strength: good; Ductile yield: very good, suitable for static installation Tensible strength: excellent Ductile yield: excellent very high elasticity, excellent creepage resistance, thus suitable for trailing cable installations Tensible stregth: very good; Ductile yield: vergy good, suitable for static installations Tensible stregth: very good; Ductile yield: good, suitable for static installation
Resistance to abrasion Good Excellent Good Good

Checklist For Selection Of Filters

What is the minimum required nominal flow rate?

See the notes in the technical data.

Are there any size restrictions?

See the notes in the design data.

Is maintenance assured?

Planning and design should permit easy maintenance.

Checklist For Selection Of Connecting Elements

Which diameter is needed?

See the design diagramm "Overview Flow Resistance in Hoses"

How long are the hoses?

The hoses recommendations are based on a hose length of 2m. For longer hoses, larger diameters must be used.

Which hose material is needed?

See the material notes. In trailing cable installations, we recommend the use of polyurethane hoses.

What are the best hose connections for the application?

For dynamic applications, you should always use unions which are secured with union nuts or hose clamps.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

액세스하려는 URL이 올바른 언어 또는 국가 컨텍스트에 맞지 않습니다.

계정에 연결된 스토어 채널이 요청된 URL의 채널과 일치하지 않습니다. 가격을 확인하거나 주문하려면 사용자별 채널로 전환하세요.

0 장바구니에 제품이 성공적으로 추가되었습니다.

장바구니로 이동