Schmalz

Selection Aid for Filters And Connectors

Overview Flow Resistance In Hoses

Aid for the dimensioning of distribution hoses:
Example: A hose with an internal diameter D = 32 mm has the same internal flow rate as 32 hoses with an internal diameter of 6 mm or 4 hoses with an internal diameter of 16 mm.

Checklist For Selection Of Hoses

Criterion/Material

PVC

PU

PE

PA

Resistance to oil

Good

Excellent

Good

Very good

Resistance to fuels and natural gas

Medium

Very good

Medium

Good

Resistance to weathering

Medium

Excellent

Medium

Medium

Behaviour at low temperatures

Freezes at -20°C

Similar to a hard plastic at -35° bis
-40°C, but no embrittlement

Freezes at -50°C

Freezes at -40°C

Behaviour at high temperatures

Withstands 70°C for long periods

Withstands 80°C for long periods, for short periods up to 100°

Withstands 70°C for long periods

Withstands 85°C for long periods

Dynamic stress resistance

Tensible strength: good; Ductile yield: very good, suitable for static installation

Tensible strength: excellent Ductile yield: excellent very high elasticity, excellent creepage resistance, thus suitable for trailing cable installations

Tensible stregth: very good; Ductile yield: vergy good, suitable for static installations

Tensible stregth: very good; Ductile yield: good, suitable for static installation

Resistance to abrasion

Good

Excellent

Good

Good

Checklist For Selection Of Filters

What is the minimum required nominal flow rate?

See the notes in the technical data.

Are there any size restrictions?

See the notes in the design data.

Is maintenance assured?

Planning and design should permit easy maintenance.

Checklist For Selection Of Connecting Elements

Which diameter is needed?

See the design diagramm "Overview Flow Resistance in Hoses"

How long are the hoses?

The hoses recommendations are based on a hose length of 2m. For longer hoses, larger diameters must be used.

Which hose material is needed?

See the material notes. In trailing cable installations, we recommend the use of polyurethane hoses.

What are the best hose connections for the application?

For dynamic applications, you should always use unions which are secured with union nuts or hose clamps.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adres URL, do którego próbujesz uzyskać dostęp, nie jest we właściwym języku lub kontekście kraju.

Kanał sklepu powiązany z Twoim kontem nie jest zgodny z kanałem żądanego adresu URL. Aby wyświetlić ceny lub złożyć zamówienie, przełącz się na kanał specyficzny dla użytkownika.

Produkt pomyślnie dodany do koszyka

Przejdź do koszyka

Schmalz Select - Preferowana gama produktów dla techniki podciśnieniowej

Wszystko dostępne. Wszystko ustawione. Wszystko jasne.

Dzięki portfolio Select można polegać na sprawdzonych, standardowych produktach, które są dostępne natychmiast i na całym świecie oraz mogą być optymalnie łączone. Koniec z długim czasem dostawy i niepewnością przy wyborze produktów. Znajdź dokładnie te części składowe, których potrzebujesz - szybko, nieskomplikowanie i dostępne na całym świecie.