Schmalz

Thin Glass Gripper

The thin glass gripper is a special gripper for the extremely dynamic and gentle handling of sensitive workpieces in automated or semi-automated processes. It reduces the dynamic and static forces on workpiece through the optimized dimensioning and distribution of suction positions.

Benefits of thin glass grippers:

  • Significant reduction in damage rate for the thinnest workpieces (less than 0.1 mm thick) 

  • Full-surface gripping with low vacuum level 

  • Suction area made from mark-free PEEK to avoid glass surface contamination

Typical areas of application:

  • Thin glass grippers are used in the manufacture of TFT displays, smartphones or tablets. The special gripper is also suitable for contamination-free handling without compromising downstream processes such as coating.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.
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
Select 포트폴리오를 사용하면 전 세계에서 즉시 사용 가능하고 최적으로 조합할 수 있는 검증된 표준 제품을 신뢰할 수 있습니다. 더 이상 긴 납품 시간과 제품 선택의 불확실성이 없습니다. 빠르고 복잡하지 않으며 전 세계에서 사용 가능한 필요한 진공 부품을 정확하게 찾아보세요.