Schmalz

Selection by Workpiece

There follow some examples of applications to assist selection of the appropriate special grippers:

Workpiece

Schmalz Special Gripper

Product

Product Properties

Solar components such as wafers and solar cells

Floating suction cups SBS

  • Low-contact handling

  • Integrated vacuum generation

 

Wafer grippers SWGm

  • Extremely fast and precise handling

  • Integrated vacuum generation with high suction rate

  • Product dimensions especially for wafer sizes 125x125 mm and 156x156 mm

Thin workpieces such as paper and foils

Floating suction cups SBS

  • Low-contact handling

  • Integrated vacuum generation

  • Absorption of lateral forces by elastomer buffer on the underside

  • Separation function during destacking

Complex steel parts such as perforated sheets and laser cut metal

Magnetic grippers SGM

  • Handling by means of a permanent magnet

  • Absorption of lateral forces by friction ring

Delicate components such as printed circuit boards

Floating suction cups SBS

  • Low-contact handling

  • Integrated vacuum generation

  • High leakage compensation

Battery components such as anodes, cathodes and separators

Composite grippers SCG

  • Integrated vacuum generation

  • Higher volume flow for a secure grip on even porous workpieces

  • Large contact surface for delicate handling

Unstable and porous workpieces such as foam and insulation materials

Needle grippers SNG

  • Needle grippers with variable needle stroke that can be adjusted for individual workpiece geometries

Fabrics that are unstable or have a "suck through" effect such as composites

Composite grippers SCG

  • Integrated vacuum generation

  • High volume flow for a secure grip on even porous workpieces

  • Large contact surface for delicate handling

 

Needle grippers SNG

  • SNG needle gripper with variable needle stroke for individual adaptation to different workpiece geometries

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.