Schmalz

Selection by Workpiece

There follow some examples of applications to assist selection of the appropriate special grippers:

Workpiece

Schmalz Special Gripper

Product

Product Properties

Solar components such as wafers and solar cells

Floating suction cups SBS

  • Low-contact handling

  • Integrated vacuum generation

 

Wafer grippers SWGm

  • Extremely fast and precise handling

  • Integrated vacuum generation with high suction rate

  • Product dimensions especially for wafer sizes 125x125 mm and 156x156 mm

Thin workpieces such as paper and foils

Floating suction cups SBS

  • Low-contact handling

  • Integrated vacuum generation

  • Absorption of lateral forces by elastomer buffer on the underside

  • Separation function during destacking

Complex steel parts such as perforated sheets and laser cut metal

Magnetic grippers SGM

  • Handling by means of a permanent magnet

  • Absorption of lateral forces by friction ring

Delicate components such as printed circuit boards

Floating suction cups SBS

  • Low-contact handling

  • Integrated vacuum generation

  • High leakage compensation

Battery components such as anodes, cathodes and separators

Composite grippers SCG

  • Integrated vacuum generation

  • Higher volume flow for a secure grip on even porous workpieces

  • Large contact surface for delicate handling

Unstable and porous workpieces such as foam and insulation materials

Needle grippers SNG

  • Needle grippers with variable needle stroke that can be adjusted for individual workpiece geometries

Fabrics that are unstable or have a "suck through" effect such as composites

Composite grippers SCG

  • Integrated vacuum generation

  • High volume flow for a secure grip on even porous workpieces

  • Large contact surface for delicate handling

 

Needle grippers SNG

  • SNG needle gripper with variable needle stroke for individual adaptation to different workpiece geometries

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.
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
Select 포트폴리오를 사용하면 전 세계에서 즉시 사용 가능하고 최적으로 조합할 수 있는 검증된 표준 제품을 신뢰할 수 있습니다. 더 이상 긴 납품 시간과 제품 선택의 불확실성이 없습니다. 빠르고 복잡하지 않으며 전 세계에서 사용 가능한 필요한 진공 부품을 정확하게 찾아보세요.