Schmalz

Overview Valves

Application

Check Valves

Flow Resistors

Sensing Valves

Handling of porous workpieces such as chipboards and MDF panels

X (If type SVN is used)

X

 

Handling of air-tight workpieces such as sheets of metal of varying sizes

X

 

X

Handling of cardboard sheets and boxes of varying sizes

 

X

 

Handling operations with very short cycle times

X

 

X

Cases where some of the suction cups are not fully in contact with the workpiece

X

X

 

Cases where the workpiece is to be blown off for faster release

X

Restricted by the reduced cross-section

Checklist For Selection Of Valves

Which functions are required?

We can supply solenoid valves (3/2-way, 2/2-way), manually actuated vacuum and compressed-air valves, check valves, sensing valves and flow resistors.

Which volume flow rate needs to be controlled?

This determines the nominal flow rate and the size of the valve.

What are the requirements with respect to size, weight and cycle times?

Further information can be found in the design data and/or technical data of the valves.

Which type of energy is available?

See the notes in the design data or the technical data (solenoid valve EMVP also needs a compressed-air supply)

Does the workpiece need to be released very quickly (blown off)?

With type EMV, compressed-air for blowing off can be connected directly. Otherwise, additional valves are needed for this function.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.