Schmalz

Small Vacuum Pump

Vacuum pumps from Schmalz are available in various sizes. The advantage of a small vacuum pump is its compact and lightweight design. The functional principle of a small vacuum pump does not differ from other vacuum pumps.

The core component of a vacuum pump is a ribbed impeller that is mounted eccentrically (A). Fresh air flows through the inlet opening (C). If the wheel rotates, the ribs are pushed outwards through the centrifugal force. When the ribs are pressed outwards, they seal chambers of different sizes (B). The rotation of the impeller and the increasing expansion of the chambers cause the air to expand and the air pressure decreases. This creates a vacuum. The compressed air flows through the outlet opening (D).

The advantage of vacuum pumps is that the substantial compression generates a high vacuum level. Pumps also have a relatively high suction rate depending on the type. Vacuum pumps are therefore particularly suited for use in packaging machines or centralized vacuum generation in gantry transfer systems. In addition, vacuum pumps are used to create vacuums in most manual vacuum handling systems.

Advantages of small vacuum pumps

  • Light and compact design

  • High vacuum with high extraction volume

  • Central vacuum generation

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.