Schmalz

Vacuum Tube Lifter JumboFlex: good becomes wow!

More simple. More efficient. More ergonomic. The tried-and-tested JumboFlex optimizes handling processes thanks to smart adaptations. Its handle fits perfectly in the hand - regardless of its size. The redesign makes the vacuum tube lifter intuitive to use and significantly reduces the training time for new skilled workers.

The optimized JumboFlex is suitable for many different hands thanks to its ergonomic design.

The JumboFlex has been the first choice for many years when it comes to moving workpieces weighing up to 50 kilograms. With its help, employees handle goods ergonomically and with a high cycle frequency. Schmalz is now proving that good things can be optimized with the redesign of the vacuum tube lifter. The new control handle is now even better suited to different hand sizes, allowing small hands to grip just as safely and fatigue-free as larger ones.

The two operating buttons are also new, replacing the single-button control. They control the up and down movement in opposite directions and are intuitive to use, allowing new employees to work productively even faster and direct the tube lifter even more precisely. If required, loads can be brought to a standstill in a floating position at any height, enabling further process steps to be carried out on the workpiece being handled. For example, labels can be easily applied or workpieces checked. The JumboFlex thus counteracts employee fatigue even more effectively than before.

Fast gripper changes with high workpiece variance for seamless processes

Thanks to the double-speed gripper change, employees handle different workpieces without interfering with handling processes. The employee can simply slide the end effector into the holder with a flick of the wrist. A simple tweezer handle for releasing the gripper enables really quick changes and prevents accidental release. If the new gripper is not properly engaged, employees receive a visual warning. A rotating mechanism, which is operated via a simple and intuitive slider, allows the workpiece being handled to be rotated 360 degrees or fixed in 90-degree increments.

When configuring the JumboFlex, users can choose between several variants and circuitry. For example, a swivelling function is available for the gripper, which can also suck in the workpiece from the side. An optional display, which is controlled via a foil keypad, informs the specialist about the weight of the goods, for example in the Weight Control version. This saves companies additional weighing, especially when picking in the dispatch area.

With the JumboFlex, companies can offer their employees an ergonomically designed work tool that makes physical work easier, reduces fatigue and increases efficiency. This enables them to position themselves as attractive employers and prevent their skilled workers and employees from leaving the company.

Thanks to the new two-button operation, the specialists control the up and down movement intuitively.

The tweezer handle enables real quick change of the gripper and prevents accidental release.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.