Schmalz

Automated handling • Packaging • Vacuum suction cups

Schmalz SG sack suction cup for handling sacks

In the past, the 20 kg sacks were handled and palletized using a claw pick-up. The claw pick-up had to be manually adjusted for each different sack type. The cycle times were also not satisfactory. Schmalz’s SG sack suction cup provided the ideal solution for this handling task.

The Schmalz SG sack suction cup picks up the sack from the surface of the workpiece and grips it securely. The suction cup is suitable for all sack types and can handle sacks with both stable and unstable contents. The sack suction cup is equipped with a special sealing foam, which allows it to precisely conform to the shape of the workpiece. A support grid within the suction cup prevents the sack from tearing or being sucked in.

With the SG sack suction cup, the output was increased from 12 to 22 pieces per minute, which enhanced the productivity of the plant by 80%.
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.