Schmalz

Schmalz Solution Kit enables bin picking at record speed

Schmalz speeds up gripping. Behind this is a solution kit that connects various software and hardware components so that robotic cells can see, grip and communicate with higher-level systems more quickly. What this can look like is demonstrated by the Pick Accelerator, which achieves top performance thanks to the ivOS Pick-and-Pack solution kit. The system will be presented for the first time at this year's LogiMAT.

The Pick Accelerator manages 2,700 picks per hour under the guidance of the Schmalz Solution Kit ivOS Pick-and-Pack.

Schmalz lifts bin picking to a new level. In order to perfect the interaction between gripper, robot, camera and picking software, the handling experts have developed the Schmalz Solution Kit, whose highlight is the open operating system ivOS. With the kit, suppliers of robotic cells - be they machine builders or integrators - receive a plug-and-work capable technology solution that is quickly integrated into any bin-picking application. At the same time, the system is so flexible and open that automation engineers can still adapt it to customer-specific requirements at any time. The complete engineering package supplied supports them in this - it includes all CAD data, circuit diagrams, technical designs and much more.

In addition, gripping technology, 3D vision sensors and a specific software configuration are part of the solution kit on request. Likewise, by integrating various interfaces, Schmalz enables communication to warehouse management systems and to various protocols, for example, to exchange data in real time. The idea behind the Solution Kit is not limited to one application scenario. In addition to the bin picking application, Schmalz is working on other picking variants.

2,700 picks per hour

Schmalz shows how the bundle can work with its Pick Accelerator. Schmalz developed a pilot application as the first use case. The Körber technology group integrated this robotic cell into the existing logistics at Schmalz's own headquarters. In it, two robots manage 2,700 picks per hour - that's picking at record speed. The robots work simultaneously and can change grippers within a second, depending on whether boxes, vials or bags are to be handled. Two 3D cameras look into the box after each pick, and the picking software analyzes this input, calculates and controls the next gripper. For the best pick, the system has several gripper algorithms available in parallel. The energy supply system is integrated into the gripper, which reaches into every corner of the crate with its five axes. As important as the individual components are, the dynamic interaction and flexibility is only made possible by the Schmalz Solution Kit ivOS Pick-and-Pack - through the unique interaction of innovative gripping technology, modern 3D sensor technology and the latest algorithms for determining the gripping point.

For the first use case, Schmalz relied on the expertise of Körber's supply chain experts. Together with Schmalz, they implemented the conveyor connection of the robotic pick-and-pack cell to the existing logistics system and the integration of the cell into the material flow control software for the pilot application. This makes Körber the first integrator to successfully install the ivOS Pick-and-Pack Solution Kit. Körber will continue to work closely with Schmalz as a sales and integration partner for bin-picking applications.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Các công ty Schmalz

Vui lòng chọn công ty Schmalz tại một trong các khu vực sau:

Các khu vực

Khu vực của bạn không có trong danh sách?

Schmalz duy trì một mạng lưới bán hàng quốc tế với các đối tác phân phối tại hơn 80 quốc gia. Vui lòng chọn ngôn ngữ cho trang web quốc tế của chúng tôi.

URL được truy cập không nằm trong bối cảnh ngôn ngữ-quốc gia phù hợp

Kênh cửa hàng được xác định dựa trên tài khoản người dùng của bạn không trùng khớp với kênh của URL đang được truy cập. Để xem giá hoặc đặt hàng, vui lòng chuyển sang kênh dành riêng cho người dùng của bạn.

0 Sản phẩm đã được thêm vào giỏ hàng thành công

Đến giỏ hàng

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.