Schmalz

From door to door

Lifting 80 kilograms 80 times in 8 hours - a Herculean task. For the highly automated industrial company Josko, vacuum expert Schmalz has therefore developed a solution that releases the task in the blink of an eye with the help of a suction spider.

The first robot picks up a blank with the suction spider and places it in front of the grinding machine.

Windows and doors not only separate interiors from the outside world, but also contribute significantly to the character of a facade or room. Whether cozy or extravagant – customer wishes are individual. At door and window expert Josko, function and design therefore go hand in hand. The company, which started out as a one-man carpentry business in 1960, generated a turnover of 215 million euros in 2022 with more than 1,000 employees. At its headquarters, idyllically located in Kopfing im Innkreis in Upper Austria, Josko produces wood, plastics/aluminum and aluminum windows, house doors and interior doors on 39,000 square meters.

The new system is designed to reduce the workload on our specialists and increase the degree of automation.
∼ Rainer Plöckinger, foreman for interior doors at the Kopfing location

Always with sustainability in mind. Josko relies on short transport routes and sources its wood primarily from local forests. Production waste is recycled or used to fuel the company's own biomass power plant. This enables the premium manufacturer to cover part of its electricity requirements from renewable resources. When it comes to employees, the focus is also on environmental protection. Josko trains skilled workers and thus keeps working distances short in the rather structurally weak region.

Ergonomics are also important to the company so as not to impair the health of its employees. Numerous systems from Schmalz support the skilled workers in handling the often heavy and bulky workpieces. On average, an interior door weighs around 70 to 80 kilograms. However, 100 kilograms is also possible. The size is variable, with a maximum width of 1.3 meters and a maximum length of three meters. In short: one person alone cannot move the sheets without a lifting aid and the job would be strenuous and stressful for two employees. Josko therefore uses different handling solutions at the individual stations.

Without manual intervention

Josko was looking for an alternative because spare parts were no longer available for the old, so-called turning system on the sanding machine. "The new system is intended to relieve our skilled workers and increase the degree of automation," emphasizes Rainer Plöckinger, Interior Doors Foreman at the Kopfing location. As Schmalz already has numerous products in production, Josko turned to the vacuum experts once again.

Together with the industrial company, Schmalz Austria set about developing a suitable system. Another requirement from Josko was that the new system should no longer require manual programming. "The WEBER KSF sanding machine, two Kuka robots and our handling solution therefore work together fully automatically," says Christian Prießner, Managing Director of Schmalz Austria.

Protected behind bars, the first robot picks up a blank from the stack and places it on a conveyor belt in front of the machine. The door leaf passes through the machine, which calibrates and grinds the surface. On the other side, the second robot picks up the blank and places it from above on a rack located between the two machines. The first robot picks it up again from the bottom, turns the door leaf and places it in front of the sanding machine again – with the reverse side facing upwards. On the second pass through the machine, the other half now also receives its finish. As soon as the processing of the front and back is complete, the second robot places the door on the "finished" stack.

A powerful grip

A suction spider from Schmalz ensures a safe grip. With significantly larger dimensions than the crawling animal and designed by the vacuum experts to meet Josko's exact requirements, one of these grippers sits on each robot arm. The low weight of the basic components made of aluminum profiles enables fast cycles, and the FMP-S gripping system with sealing foam is perfect for handling heavy and rough workpieces such as door leaves. Vacuum generation takes place via a connector to the compressed air network and is controlled by valves. Thanks to the integrated system monitoring and sensor technology, the suction spiders work with absolute process reliability.

The interaction between the robot and gripper moves around 70 to 80 door leaves per day, which pass through the workstation in an eight-hour shift. Since the start of operations in 2020, the system has processed round 50,000 blanks - fully automatically and ergonomically, without burdening employees with strenuous activities such as moving the heavy elements. "We are more than satisfied with the solution," emphasizes Plöckinger. "Only if the power fails, the machine comes to a standstill," he says with a wink. But fortunately, that hasn't happened yet. The highlight for the staff: individual dimensions are stored in the system for different blanks, which the specialists simply select via the display. Manual programming is finally a thing of the past. "We have also eliminated a potential source of errors," adds Plöckinger happily.

The suction spider holds door leaves with a maximum length of three meters and a weight of up to 100 kilograms.

The sanding machine smoothes between 70 and 80 door leaves per day on the front and back.

Thanks to the modular principle, the suction spider can be adapted to individual requirements.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku