Schmalz

VacuMaster Charge: ergonomics without a power socket

How can the flexibility of the vacuum lifting device VacuMaster be further increased? Vacuum expert Schmalz has a simple answer to this question: with a rechargeable battery. This enables professionals to work ergonomically without mains power.

Independent of a power supply, the VacuMaster Charge transports workpieces weighing up to 750 kilograms.

The VacuMaster has become an indispensable tool in metal and woodworking operations. Thanks to many equipment variants, the vacuum lifting device adapts to all requirements. It transports unwieldy workpieces such as sheet metal or wooden boards. With the new VacuMaster Charge, skilled workers now also handle loads independently of a power supply. This increases flexibility, as only an overhead crane is required, but no connector to the power supply. Another advantage: after the work is done, the lifting aid is quickly put down and the crane system is ready for other services.

The VacuMaster Charge has a battery that provides enough power for an eight-hour shift in normal operation. Longer shifts are no problem with an optional exchangeable battery: This allows employees to use the lifting device continuously over several shifts. The power storage unit supplies four diaphragm pumps with energy. Users have a suction rate of eight cubic meters per hour and a vacuum of -850 millibars at their disposal. The intelligent control system switches off the four pumps when the vacuum level is safe and thus guarantees low energy consumption and long battery life.

Developed in the standard version for horizontal transport of suction-tight workpieces, specialists also handle diamond plates safely with special suction plates. The VacuMaster Charge can handle loads of up to 750 kilograms. The modular system allows users to adapt the battery-powered lifting device to individual requirements, as is the case with all models in the product family.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku