Schmalz

Ruční manipulace • Kov / plech • Plechy • Vakuové zvedáky trubek JumboErgo

The Vacuum Tube Lifter JumboErgo Enables to Unload a CNC Production Line without Damaging the Materials

Wall elements are manufactured from sheet metal in a CNC production line. The unloading of the line is carried out by two employees. In addition to the pure unloading and commissioning of the line, work simplification, commissioning and the protection of the sensitive sheet metal parts were of high importance.

The vacuum tube lifter JumboErgo45 is designed for horizontal handling of workpieces weighing up to 45 kg. Efficient machine unloading by just one person reduces machine downtimes and increases productivity. In addition, the holding and lifting process, which is realized exclusively via the medium of vacuum, guarantees material-protecting and scratch-free work. The tube lifter is equipped with a double suction pad. Both suction pads can be continuously adjusted to the respective workpiece format on the longitudinal crosshead. In this application, the vacuum tube lifter JumboErgo is combined with a column-mounted slewing crane SK made of aluminum for loads up to 110 kg. The very smooth-running crane system enables particularly ergonomic operation of the vacuum tube lifter and rounds off the Schmalz solution very well.

Zobrazit více
Product Inquiry

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku