The Vacuum Tube Lifter JumboFlex Simplifies the Loading and Unloading of Passenger Luggage and Freight at Münster-Osnabrück Airport
Ground handling (unloading pieces of luggage) used to be performed by hand. This work demanded an enormous physical effort on the part of the employees. Suitcases weighing as much as 30 kg are routed along a conveyor belt to the specific chute that is defined for a given flight number. The pieces of luggage are then placed onto the apron trolley or transport trolley by an employee. From there the pieces of baggage are brought to the airplanes. The Schmalz company was confronted with the requirements of the workload, the low room height, and different types of baggage, such as trolleys, hard-shell suitcases, and sports bags. Ergonomic Handling Solutions
The vacuum tube lifter JumboFlex is ideal for frequent, very fast movement of lightweight baggages (up to 35 kg). Its numerous features provide crucial advantages for handling passenger baggage and special baggage. The vacuum tube lifter’s ergonomic, single-hand operation simplifies the work to be done by one person, without endangering the employee’s health. The 2-in-1 gripper has a simple rotating mechanism that allows the user to switch from the vacuum baggage gripper to a mechanical single-hook head for pieces of baggage that cannot be held using suction. A special crane system with a crane length of 6,000 mm rounds off this complete solution. It ensures perfect low-friction operation, is optimally geared for low room heights, and is the perfect complement to the vacuum tube lifter JumboFlex.
Videa
Objevte příklady použití produktu v různých odvětvích - uživatelsky přívětivé, informativní a praktické.
Nebyla nalezena žádná vhodná videa? Pak se podívejte do našeho mediálního centra.