Vacuum Lifting Devices VacuMaster Eco
- VacuMaster Eco for operation without an external power source
- For airtight workpieces
- Lift capacities up to 1,000 kg
To process aluminum plates weighing up to 250 kg on a CNC machine tool, loading used to be done by hand. This task required at least two employees. To relieve the strain on these employees and protect their health, the company decided to make a change.
The vacuum lifting device VacuMaster Eco provided the perfect solution for horizontally lifting the aluminum and metal plates and depositing them for the CNC machine tool. The advantages of the VacuMaster Eco lifting device include that it does not require an external energy source. This means that this lifting aid is especially flexible in use. The battery-operated warning device with battery test function ensures a high degree of work safety. In this case, the vacuum lifting device was designed for a maximum load of 250 kg and can be operated by one person. The company is thrilled about the resulting 50% reduction in personnel costs and highly satisfied.
Objevte příklady použití produktu v různých odvětvích - uživatelsky přívětivé, informativní a praktické.
Nebyla nalezena žádná vhodná videa? Pak se podívejte do našeho mediálního centra.